Tool/software:
I'm working on a design where VIO is 3.3v and none of the 1.8V specific peripherals are used. Is VIOIN_18 still required, or can it be unconnected or somehow disabled?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
I'm working on a design where VIO is 3.3v and none of the 1.8V specific peripherals are used. Is VIOIN_18 still required, or can it be unconnected or somehow disabled?
Hi Corey,
The VIOIN_18 is used internally in the AM273x device, so it is a required power rail, even if all GPIOs are run at 3.3V (using 3.3V on VIOIN).
Thanks,
Mike
Thanks a bunch, this is what I needed to know. I was hoping to remove some power converters.