This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM62P: Can I signed on a build image?

Part Number: AM62P


Tool/software:

Hi,Team
I wonder if I can signed on a

mcu_r5_image build by others?

Thank you for your support.

Best Regards, KONG XIANGXU

  • Hello,

    The following script is used for signing the application images:

    https://github.com/TexasInstruments/mcupsdk-core-k3/blob/k3_next/tools/boot/signing/appimage_x509_cert_gen.py#L1-L1

    This can be used as a standalone script outside of the build procedure to sign the generate application binaries.

    Regards,

    Prashant

  • # arguments definition
    my_parser = argparse.ArgumentParser(description="Generates a x509 certificate for an application binary to boot it in HS device")
    
    my_parser.add_argument('--bin',        type=str, help='Bin file that needs to be signed')
    my_parser.add_argument('--key',        type=str, help='File with signing key inside it')
    my_parser.add_argument('--enckey',     type=str, help='File with encryption key inside it')
    my_parser.add_argument('--cert',       type=str, help='Certificate file name (optional, will use a default name otherwise)')
    my_parser.add_argument('--output',     type=str, help='Output file name (concatenated cert+bin)')
    my_parser.add_argument('--core',       type=str, help='Core on which the binary is meant to be loaded. Optional')
    my_parser.add_argument('--enc',        type=str, help='If the binary need to be encrypted or not [y/n]')
    my_parser.add_argument('--loadaddr',   type=str, help='Target load address of the binary in hex. Default to 0x70000000')
    my_parser.add_argument('--authtype',   type=str, help='Authentication type. [0/1/2]. 0 - Move to destination address specified after authentication, 1 - In place authentication, 2 - Move to the certificate start after authentication. Default is 1')
    my_parser.add_argument('--keyversion', type=str, help='App signing key version. [1.5/2.2]. 1.5 - RSASSA PKCS v1.5 schem

    Can you give me an example on how to fill  these argus?

  • The makefile of any example can be referred for the signing command:

    github.com/.../makefile