Tool/software:
Hello,
I have a question that I need your advice on: When using the AM6422, running the FreeRTOS system on the R5F core alone, three external interrupts work normally. However, when using Linux to boot the R5F, the external interrupts become unresponsive, while timer interrupts function properly. What could be the reason for this?I can confirm that there is no conflict in pin resources.Below is my device tree file. The external interrupt pins used in the R5F are U13 (GPIO0_52), T1 (GPIO1_7), and U9 (GPIO0_57).
// SPDX-License-Identifier: GPL-2.0 /* * Copyright (C) 2020-2021 Texas Instruments Incorporated - https://www.ti.com/ */ /dts-v1/; #include <dt-bindings/phy/phy.h> #include <dt-bindings/mux/ti-serdes.h> #include <dt-bindings/leds/common.h> #include <dt-bindings/gpio/gpio.h> #include <dt-bindings/net/ti-dp83867.h> #include "k3-am642.dtsi" / { compatible = "ti,am642-evm", "ti,am642"; model = "Texas Instruments AM642 EVM"; chosen { stdout-path = "serial2:115200n8"; bootargs = "console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000"; }; aliases { ethernet2 = &icssg0_emac0; ethernet3 = &icssg0_emac1; }; memory@80000000 { device_type = "memory"; /* 2G RAM */ reg = <0x00000000 0x80000000 0x00000000 0x80000000>; }; reserved-memory { #address-cells = <2>; #size-cells = <2>; ranges; secure_ddr: optee@9e800000 { reg = <0x00 0x9e800000 0x00 0x01800000>; /* for OP-TEE */ alignment = <0x1000>; no-map; }; main_r5fss0_core0_dma_memory_region: r5f-dma-memory@a0000000 { compatible = "shared-dma-pool"; reg = <0x00 0xa0000000 0x00 0x100000>; no-map; }; main_r5fss0_core0_memory_region: r5f-memory@a0100000 { compatible = "shared-dma-pool"; reg = <0x00 0xa0100000 0x00 0xf00000>; no-map; }; // main_r5fss0_core1_dma_memory_region: r5f-dma-memory@a1000000 { // compatible = "shared-dma-pool"; // reg = <0x00 0xa1000000 0x00 0x100000>; // no-map; // }; // // main_r5fss0_core1_memory_region: r5f-memory@a1100000 { // compatible = "shared-dma-pool"; // reg = <0x00 0xa1100000 0x00 0xf00000>; // no-map; // }; main_r5fss1_core0_dma_memory_region: r5f-dma-memory@a2000000 { compatible = "shared-dma-pool"; reg = <0x00 0xa2000000 0x00 0x100000>; no-map; }; main_r5fss1_core0_memory_region: r5f-memory@a2100000 { compatible = "shared-dma-pool"; reg = <0x00 0xa2100000 0x00 0xf00000>; no-map; }; // main_r5fss1_core1_dma_memory_region: r5f-dma-memory@a3000000 { // compatible = "shared-dma-pool"; // reg = <0x00 0xa3000000 0x00 0x100000>; // no-map; // }; // // main_r5fss1_core1_memory_region: r5f-memory@a3100000 { // compatible = "shared-dma-pool"; // reg = <0x00 0xa3100000 0x00 0xf00000>; // no-map; // }; mcu_m4fss_dma_memory_region: m4f-dma-memory@a4000000 { compatible = "shared-dma-pool"; reg = <0x00 0xa4000000 0x00 0x100000>; no-map; }; mcu_m4fss_memory_region: m4f-memory@a4100000 { compatible = "shared-dma-pool"; reg = <0x00 0xa4100000 0x00 0xf00000>; no-map; }; rtos_ipc_memory_region: ipc-memories@a5000000 { reg = <0x00 0xa5000000 0x00 0x00800000>; alignment = <0x1000>; no-map; }; }; icssg0_eth: icssg0-eth { compatible = "ti,am642-icssg-prueth"; pinctrl-names = "default"; pinctrl-0 = <&icssg0_rgmii1_pins_default &icssg0_rgmii2_pins_default>; sram = <&oc_sram>; ti,prus = <&pru0_0>, <&rtu0_0>, <&tx_pru0_0>, <&pru0_1>, <&rtu0_1>, <&tx_pru0_1>; firmware-name = "ti-pruss/am65x-sr2-pru0-prueth-fw.elf", "ti-pruss/am65x-sr2-rtu0-prueth-fw.elf", "ti-pruss/am65x-sr2-txpru0-prueth-fw.elf", "ti-pruss/am65x-sr2-pru1-prueth-fw.elf", "ti-pruss/am65x-sr2-rtu1-prueth-fw.elf", "ti-pruss/am65x-sr2-txpru1-prueth-fw.elf"; ti,pruss-gp-mux-sel = <2>, /* MII mode */ <2>, <2>, <2>, /* MII mode */ <2>, <2>; mii-g-rt = <&icssg0_mii_g_rt>; mii-rt = <&icssg0_mii_rt>; iep = <&icssg0_iep0>, <&icssg0_iep1>; interrupt-parent = <&icssg0_intc>; interrupts = <24 0 2>, <25 1 3>; interrupt-names = "tx_ts0", "tx_ts1"; dmas = <&main_pktdma 0xc100 15>, /* egress slice 0 */ <&main_pktdma 0xc101 15>, /* egress slice 0 */ <&main_pktdma 0xc102 15>, /* egress slice 0 */ <&main_pktdma 0xc103 15>, /* egress slice 0 */ <&main_pktdma 0xc104 15>, /* egress slice 1 */ <&main_pktdma 0xc105 15>, /* egress slice 1 */ <&main_pktdma 0xc106 15>, /* egress slice 1 */ <&main_pktdma 0xc107 15>, /* egress slice 1 */ <&main_pktdma 0x4100 15>, /* ingress slice 0 */ <&main_pktdma 0x4101 15>, /* ingress slice 1 */ <&main_pktdma 0x4102 0>, /* mgmnt rsp slice 0 */ <&main_pktdma 0x4103 0>; /* mgmnt rsp slice 1 */ dma-names = "tx0-0", "tx0-1", "tx0-2", "tx0-3", "tx1-0", "tx1-1", "tx1-2", "tx1-3", "rx0", "rx1", "rxmgm0", "rxmgm1"; icssg0_emac0: ethernet-mii0 { status = "okay"; phy-handle = <&icssg0_phy1>; phy-mode = "rgmii-rxid"; syscon-rgmii-delay = <&main_conf 0x4110>; /* Filled in by bootloader */ local-mac-address = [12 e1 7d f8 a3 e7]; }; icssg0_emac1: ethernet-mii1 { status = "okay"; phy-handle = <&icssg0_phy2>; phy-mode = "rgmii-rxid"; syscon-rgmii-delay = <&main_conf 0x4114>; /* Filled in by bootloader */ local-mac-address = [12 e1 7d f8 a3 e6]; }; }; // leds { // compatible = "gpio-leds"; // pinctrl-names = "default"; // pinctrl-0 = <&usr_led_pins_default>; // // led-0 { // label = "am64-evm:green:heartbeat"; // gpios = <&main_gpio1 44 GPIO_ACTIVE_HIGH>; // linux,default-trigger = "heartbeat"; // function = LED_FUNCTION_HEARTBEAT; // default-state = "off"; // }; // }; }; &main_r5fss0_core0 { mboxes = <&mailbox0_cluster2 &mbox_main_r5fss0_core0>; memory-region = <&main_r5fss0_core0_dma_memory_region>, <&main_r5fss0_core0_memory_region>; }; //&main_r5fss0_core1 { // mboxes = <&mailbox0_cluster2 &mbox_main_r5fss0_core1>; // memory-region = <&main_r5fss0_core1_dma_memory_region>, // <&main_r5fss0_core1_memory_region>; //}; &main_r5fss1_core0 { mboxes = <&mailbox0_cluster4 &mbox_main_r5fss1_core0>; memory-region = <&main_r5fss1_core0_dma_memory_region>, <&main_r5fss1_core0_memory_region>; }; //&main_r5fss1_core1 { // mboxes = <&mailbox0_cluster4 &mbox_main_r5fss1_core1>; // memory-region = <&main_r5fss1_core1_dma_memory_region>, // <&main_r5fss1_core1_memory_region>; //}; &mcu_m4fss { mboxes = <&mailbox0_cluster6 &mbox_m4_0>; memory-region = <&mcu_m4fss_dma_memory_region>, <&mcu_m4fss_memory_region>; }; &main_pmx0 { main_mmc1_pins_default: main-mmc1-pins-default { pinctrl-single,pins = < AM64X_IOPAD(0x0294, PIN_INPUT, 0) /* (J19) MMC1_CMD */ AM64X_IOPAD(0x0290, PIN_INPUT, 0) /* (#N/A) MMC1_CLKLB */ AM64X_IOPAD(0x028c, PIN_INPUT, 0) /* (L20) MMC1_CLK */ AM64X_IOPAD(0x0288, PIN_INPUT, 0) /* (K21) MMC1_DAT0 */ AM64X_IOPAD(0x0284, PIN_INPUT, 0) /* (L21) MMC1_DAT1 */ AM64X_IOPAD(0x0280, PIN_INPUT, 0) /* (K19) MMC1_DAT2 */ AM64X_IOPAD(0x027c, PIN_INPUT, 0) /* (K18) MMC1_DAT3 */ AM64X_IOPAD(0x0298, PIN_INPUT, 0) /* (D19) MMC1_SDCD */ >; }; main_uart0_pins_default: main-uart0-pins-default { pinctrl-single,pins = < AM64X_IOPAD(0x0230, PIN_INPUT, 0) /* (D15) UART0_RXD */ AM64X_IOPAD(0x0234, PIN_OUTPUT, 0) /* (C16) UART0_TXD */ >; }; main_uart1_pins_default: main-uart1-pins-default { pinctrl-single,pins = < AM64X_IOPAD(0x0240, PIN_INPUT, 0) /* (E15) UART1_RXD */ AM64X_IOPAD(0x0244, PIN_OUTPUT, 0) /* (E14) UART1_TXD */ >; }; main_uart2_pins_default: main-uart2-pins-default { pinctrl-single,pins = < AM64X_IOPAD(0x01A8, PIN_INPUT, 10) /* (V1) UART2_RXD */ AM64X_IOPAD(0x023c, PIN_OUTPUT, 3) /* (A16) UART2_TXD UART0_RTSn*/ >; }; main_uart3_pins_default: main-uart3-pins-default { pinctrl-single,pins = < AM64X_IOPAD(0x01AC, PIN_INPUT, 10) /* (W1) UART3_RXD PRG0_PRU0_GPO19*/ AM64X_IOPAD(0x024c, PIN_OUTPUT, 4) /* (E16) UART3_TXD UART1_RTSn*/ >; }; // icssg0_iep0_pins_default: icssg0-iep0-pins-default { // pinctrl-single,pins = < // AM64X_IOPAD(0x01AC, PIN_OUTPUT, 2) /* (W1) UART3_RXD PRG0_PRU0_GPO19*/ // >; // }; // mdio1_pins_default: mdio1-pins-default { // pinctrl-single,pins = < // AM64X_IOPAD(0x01fc, PIN_OUTPUT, 4) /* (R2) PRG0_PRU1_GPO19.MDIO0_MDC */ // AM64X_IOPAD(0x01f8, PIN_INPUT, 4) /* (P5) PRG0_PRU1_GPO18.MDIO0_MDIO */ // >; // }; // di_do_pins_default: di-do-pins-default { // pinctrl-single,pins = < // AM64X_IOPAD(0x00D0, PIN_INPUT, 7) /* (AA7) PRG1_PRU0_GPO6 GPIO0_51 */ // AM64X_IOPAD(0x00c8, PIN_INPUT, 7) /* (Y8) PRG1_PRU0_GPO4 GPIO0_49 */ // AM64X_IOPAD(0x00C4, PIN_INPUT, 7) /* (V8) PRG1_PRU0_GPO3 GPIO0_48 */ // AM64X_IOPAD(0x00C0, PIN_INPUT, 7) /* (W8) PRG1_PRU0_GPO2 GPIO0_47 */ // AM64X_IOPAD(0x00B8, PIN_OUTPUT, 7) /* (Y7) PRG1_PRU0_GPO0 GPIO0_45 */ // AM64X_IOPAD(0x00BC, PIN_OUTPUT, 7) /* (U8) PRG1_PRU0_GPO1 GPIO0_46 */ // AM64X_IOPAD(0x010c, PIN_OUTPUT, 7) /* (V11) PRG1_PRU1_GPO1 GPIO0_66 */ // >; // }; // net_rst_pin_default:net-rst-pin-default{ // pinctrl-single,pins = < // AM64X_IOPAD(0x01c4, PIN_OUTPUT, 7) /* (P4) PRG0_PRU1_GPO5 GPIO1_25 */ // AM64X_IOPAD(0x0174, PIN_OUTPUT, 7) /* (R3) PRG0_PRU0_GPO5 GPIO1_5 */ // >; // }; // rgmii1_pins_default: rgmii1-pins-default { // pinctrl-single,pins = < // AM64X_IOPAD(0x011c, PIN_INPUT, 4) /* (AA13) PRG1_PRU1_GPO5.RGMII1_RD0 */ // AM64X_IOPAD(0x0128, PIN_INPUT, 4) /* (U12) PRG1_PRU1_GPO8.RGMII1_RD1 */ // AM64X_IOPAD(0x0150, PIN_INPUT, 4) /* (Y13) PRG1_PRU1_GPO18.RGMII1_RD2 */ // AM64X_IOPAD(0x0154, PIN_INPUT, 4) /* (V12) PRG1_PRU1_GPO19.RGMII1_RD3 */ // AM64X_IOPAD(0x00d8, PIN_INPUT, 4) /* (W13) PRG1_PRU0_GPO8.RGMII1_RXC */ // AM64X_IOPAD(0x00cc, PIN_INPUT, 4) /* (V13) PRG1_PRU0_GPO5.RGMII1_RX_CTL */ // AM64X_IOPAD(0x0124, PIN_OUTPUT, 4) /* (V15) PRG1_PRU1_GPO7.RGMII1_TD0 */ // AM64X_IOPAD(0x012c, PIN_OUTPUT, 4) /* (V14) PRG1_PRU1_GPO9.RGMII1_TD1 */ // AM64X_IOPAD(0x0130, PIN_OUTPUT, 4) /* (W14) PRG1_PRU1_GPO10.RGMII1_TD2 */ // AM64X_IOPAD(0x014c, PIN_OUTPUT, 4) /* (AA14) PRG1_PRU1_GPO17.RGMII1_TD3 */ // AM64X_IOPAD(0x00e0, PIN_OUTPUT, 4) /* (U14) PRG1_PRU0_GPO10.RGMII1_TXC */ // AM64X_IOPAD(0x00dc, PIN_OUTPUT, 4) /* (U15) PRG1_PRU0_GPO9.RGMII1_TX_CTL */ // >; // }; // // rgmii2_pins_default: rgmii2-pins-default { // pinctrl-single,pins = < // AM64X_IOPAD(0x0108, PIN_INPUT, 4) /* (W11) PRG1_PRU1_GPO0.RGMII2_RD0 */ // AM64X_IOPAD(0x010c, PIN_INPUT, 4) /* (V11) PRG1_PRU1_GPO1.RGMII2_RD1 */ // AM64X_IOPAD(0x0110, PIN_INPUT, 4) /* (AA12) PRG1_PRU1_GPO2.RGMII2_RD2 */ // AM64X_IOPAD(0x0114, PIN_INPUT, 4) /* (Y12) PRG1_PRU1_GPO3.RGMII2_RD3 */ // AM64X_IOPAD(0x0120, PIN_INPUT, 4) /* (U11) PRG1_PRU1_GPO6.RGMII2_RXC */ // AM64X_IOPAD(0x0118, PIN_INPUT, 4) /* (W12) PRG1_PRU1_GPO4.RGMII2_RX_CTL */ // AM64X_IOPAD(0x0134, PIN_OUTPUT, 4) /* (AA10) PRG1_PRU1_GPO11.RGMII2_TD0 */ // AM64X_IOPAD(0x0138, PIN_OUTPUT, 4) /* (V10) PRG1_PRU1_GPO12.RGMII2_TD1 */ // AM64X_IOPAD(0x013c, PIN_OUTPUT, 4) /* (U10) PRG1_PRU1_GPO13.RGMII2_TD2 */ // AM64X_IOPAD(0x0140, PIN_OUTPUT, 4) /* (AA11) PRG1_PRU1_GPO14.RGMII2_TD3 */ // AM64X_IOPAD(0x0148, PIN_OUTPUT, 4) /* (Y10) PRG1_PRU1_GPO16.RGMII2_TXC */ // AM64X_IOPAD(0x0144, PIN_OUTPUT, 4) /* (Y11) PRG1_PRU1_GPO15.RGMII2_TX_CTL */ // >; // }; icssg0_mdio0_pins_default: icssg0_mdio_pins_default { pinctrl-single,pins = < AM64X_IOPAD(0x0204, PIN_OUTPUT, 0) /* (P3) PRG0_MDIO0_MDC */ AM64X_IOPAD(0x0200, PIN_INPUT, 0) /* (P2) PRG0_MDIO0_MDIO */ >; }; icssg0_rgmii1_pins_default: icssg0-rgmii1-pins-default { pinctrl-single,pins = < AM64X_IOPAD(0x0160, PIN_INPUT, 2) /* (Y1) PRG0_PRU0_GPO0.PRG0_RGMII1_RD0 */ AM64X_IOPAD(0x0164, PIN_INPUT, 2) /* (R4) PRG0_PRU0_GPO1.PRG0_RGMII1_RD1 */ AM64X_IOPAD(0x0168, PIN_INPUT, 2) /* (U2) PRG0_PRU0_GPO2.PRG0_RGMII1_RD2 */ AM64X_IOPAD(0x016c, PIN_INPUT, 2) /* (V2) PRG0_PRU0_GPO3.PRG0_RGMII1_RD3 */ AM64X_IOPAD(0x0178, PIN_INPUT, 2) /* (T3) PRG0_PRU0_GPO6.PRG0_RGMII1_RXC */ AM64X_IOPAD(0x0170, PIN_INPUT, 2) /* (AA2) PRG0_PRU0_GPO4.PRG0_RGMII1_RX_CTL */ AM64X_IOPAD(0x018c, PIN_OUTPUT, 2) /* (Y3) PRG0_PRU0_GPO11.PRG0_RGMII1_TD0 */ AM64X_IOPAD(0x0190, PIN_OUTPUT, 2) /* (AA3) PRG0_PRU0_GPO12.PRG0_RGMII1_TD1 */ AM64X_IOPAD(0x0194, PIN_OUTPUT, 2) /* (R6) PRG0_PRU0_GPO13.PRG0_RGMII1_TD2 */ AM64X_IOPAD(0x0198, PIN_OUTPUT, 2) /* (V4) PRG0_PRU0_GPO14.PRG0_RGMII1_TD3 */ AM64X_IOPAD(0x01a0, PIN_OUTPUT, 2) /* (U4) PRG0_PRU0_GPO16.PRG0_RGMII1_TXC */ AM64X_IOPAD(0x019c, PIN_OUTPUT, 2) /* (T5) PRG0_PRU0_GPO15.PRG0_RGMII1_TX_CTL */ >; }; icssg0_rgmii2_pins_default: icssg0-rgmii2-pins-default { pinctrl-single,pins = < AM64X_IOPAD(0x01b0, PIN_INPUT, 2) /* (Y2) PRG0_PRU1_GPO0.PRG0_RGMII2_RD0 */ AM64X_IOPAD(0x01b4, PIN_INPUT, 2) /* (W2) PRG0_PRU1_GPO1.PRG0_RGMII2_RD1 */ AM64X_IOPAD(0x01b8, PIN_INPUT, 2) /* (V3) PRG0_PRU1_GPO2.PRG0_RGMII2_RD2 */ AM64X_IOPAD(0x01bc, PIN_INPUT, 2) /* (T4) PRG0_PRU1_GPO3.PRG0_RGMII2_RD3 */ AM64X_IOPAD(0x01c8, PIN_INPUT, 2) /* (R5) PRG0_PRU1_GPO6.PRG0_RGMII2_RXC */ AM64X_IOPAD(0x01c0, PIN_INPUT, 2) /* (W3) PRG0_PRU1_GPO4.PRG0_RGMII2_RX_CTL */ AM64X_IOPAD(0x01dc, PIN_OUTPUT, 2) /* (W4) PRG0_PRU1_GPO11.PRG0_RGMII2_TD0 */ AM64X_IOPAD(0x01e0, PIN_OUTPUT, 2) /* (Y4) PRG0_PRU1_GPO12.PRG0_RGMII2_TD1 */ AM64X_IOPAD(0x01e4, PIN_OUTPUT, 2) /* (T6) PRG0_PRU1_GPO13.PRG0_RGMII2_TD2 */ AM64X_IOPAD(0x01e8, PIN_OUTPUT, 2) /* (U6) PRG0_PRU1_GPO14.PRG0_RGMII2_TD3 */ AM64X_IOPAD(0x01f0, PIN_OUTPUT, 2) /* (AA4) PRG0_PRU1_GPO16.PRG0_RGMII2_TXC */ AM64X_IOPAD(0x01ec, PIN_OUTPUT, 2) /* (U5) PRG0_PRU1_GPO15.PRG0_RGMII2_TX_CTL */ >; }; ospi0_pins_default: ospi0-pins-default { pinctrl-single,pins = < AM64X_IOPAD(0x0000, PIN_OUTPUT, 0) /* (N20) OSPI0_CLK */ AM64X_IOPAD(0x002c, PIN_OUTPUT, 0) /* (L19) OSPI0_CSn0 */ AM64X_IOPAD(0x000c, PIN_INPUT, 0) /* (M19) OSPI0_D0 */ AM64X_IOPAD(0x0010, PIN_INPUT, 0) /* (M18) OSPI0_D1 */ AM64X_IOPAD(0x0014, PIN_INPUT, 0) /* (M20) OSPI0_D2 */ AM64X_IOPAD(0x0018, PIN_INPUT, 0) /* (M21) OSPI0_D3 */ AM64X_IOPAD(0x001c, PIN_INPUT, 0) /* (P21) OSPI0_D4 */ AM64X_IOPAD(0x0020, PIN_INPUT, 0) /* (P20) OSPI0_D5 */ AM64X_IOPAD(0x0024, PIN_INPUT, 0) /* (N18) OSPI0_D6 */ AM64X_IOPAD(0x0028, PIN_INPUT, 0) /* (M17) OSPI0_D7 */ AM64X_IOPAD(0x0008, PIN_INPUT, 0) /* (N19) OSPI0_DQS */ >; }; main_usb0_pins_default: main-usb0-pins-default { pinctrl-single,pins = < AM64X_IOPAD(0x02a8, PIN_OUTPUT, 0) /* (E19) USB0_DRVVBUS */ >; }; // usr_led_pins_default: usr-led-pins-default { // pinctrl-single,pins = < // AM64X_IOPAD(0x210, PIN_OUTPUT, 7) /* (D13) PRG1_PRU0_GPO15.GPIO1_44 */ // >; // }; }; &main_gpio0 { status = "disable"; // pinctrl-names = "default"; // pinctrl-0 = <&di_do_pins_default>; // status = "okay"; }; &main_gpio1 { status = "disable"; // pinctrl-names = "default"; // pinctrl-0 = <&net_rst_pin_default>; // status = "okay"; }; &main_uart0 { pinctrl-names = "default"; pinctrl-0 = <&main_uart0_pins_default>; }; /* main_uart1 is reserved for firmware usage */ &main_uart1 { pinctrl-names = "default"; pinctrl-0 = <&main_uart1_pins_default>; }; &main_uart2 { pinctrl-names = "default"; pinctrl-0 = <&main_uart2_pins_default>; }; &main_uart3 { pinctrl-names = "default"; pinctrl-0 = <&main_uart3_pins_default>; }; &main_uart4 { status = "disabled"; }; &main_uart5 { status = "disabled"; }; &main_uart6 { status = "disabled"; }; &mcu_uart0 { status = "disabled"; }; &mcu_uart1 { status = "disabled"; }; &main_i2c1 { status = "disabled"; }; /* mcu_gpio0 is reserved for mcu firmware usage */ &mcu_gpio0 { status = "reserved"; }; &mcu_i2c0 { status = "disabled"; }; &main_i2c0 { status = "disabled"; }; &main_i2c2 { status = "disabled"; }; &main_i2c3 { status = "disabled"; }; &mcu_i2c1 { status = "disabled"; }; &mcu_spi0 { status = "disabled"; }; &mcu_spi1 { status = "disabled"; }; &main_spi0 { status = "disabled"; }; &sdhci0 { /* emmc */ bus-width = <8>; non-removable; ti,driver-strength-ohm = <50>; disable-wp; }; &sdhci1 { /* SD/MMC */ pinctrl-names = "default"; bus-width = <4>; pinctrl-0 = <&main_mmc1_pins_default>; ti,driver-strength-ohm = <50>; disable-wp; no-1-8-v; }; &usbss0 { ti,vbus-divider; ti,usb2-only; }; &usb0 { dr_mode = "host";//"otg"; maximum-speed = "high-speed"; pinctrl-names = "default"; pinctrl-0 = <&main_usb0_pins_default>; }; &cpsw3g { status = "disabled"; // pinctrl-names = "default"; // pinctrl-0 = <&mdio1_pins_default // &rgmii1_pins_default // &rgmii2_pins_default>; //// cpts@3d000 { //// ti,pps = <7 1>; //// }; }; //&cpsw_port1 { // phy-mode = "rgmii-rxid"; // phy-handle = <&cpsw3g_phy0>; //}; // //&cpsw_port2 { // phy-mode = "rgmii-rxid"; // phy-handle = <&cpsw3g_phy1>; //}; &cpsw3g_mdio { status = "disabled"; // cpsw3g_phy0: ethernet-phy@1 { // reg = <1>; // ti,rx-internal-delay = <DP83867_RGMIIDCTL_2_00_NS>; // ti,fifo-depth = <DP83867_PHYCR_FIFO_DEPTH_4_B_NIB>; // }; // // cpsw3g_phy1: ethernet-phy@0 { // reg = <0>; // ti,rx-internal-delay = <DP83867_RGMIIDCTL_2_00_NS>; // ti,fifo-depth = <DP83867_PHYCR_FIFO_DEPTH_4_B_NIB>; // }; }; //#define TS_OFFSET(pa, val) (0x4+(pa)*4) (0x10000 | val) // //×ync_router { // pinctrl-names = "default"; // pinctrl-0 = <&mcu_cpts_pps>; // // /* Example of the timesync routing */ // mcu_cpts_pps: mcu-cpts-pps { // pinctrl-single,pins = < // /* pps [cpts genf1] in22 -> out37 [cpts hw8_push] */ // TS_OFFSET(37, 22) // /* pps [cpts genf1] in22 -> out25 [SYNC1_OUT pin] */ // TS_OFFSET(25, 22) // >; // }; //}; /* set R5F subsystem 0 to single-CPU mode */ &main_r5fss0 { ti,cluster-mode = <2>; }; &main_r5fss1 { ti,cluster-mode = <2>; }; &mailbox0_cluster2 { mbox_main_r5fss0_core0: mbox-main-r5fss0-core0 { ti,mbox-rx = <0 0 2>; ti,mbox-tx = <1 0 2>; }; // mbox_main_r5fss0_core1: mbox-main-r5fss0-core1 { // ti,mbox-rx = <2 0 2>; // ti,mbox-tx = <3 0 2>; // }; }; &mailbox0_cluster3 { status = "disabled"; }; &mailbox0_cluster4 { mbox_main_r5fss1_core0: mbox-main-r5fss1-core0 { ti,mbox-rx = <0 0 2>; ti,mbox-tx = <1 0 2>; }; // mbox_main_r5fss1_core1: mbox-main-r5fss1-core1 { // ti,mbox-rx = <2 0 2>; // ti,mbox-tx = <3 0 2>; // }; }; &mailbox0_cluster5 { status = "disabled"; }; &mailbox0_cluster6 { mbox_m4_0: mbox-m4-0 { ti,mbox-rx = <0 0 2>; ti,mbox-tx = <1 0 2>; }; }; &mailbox0_cluster7 { status = "disabled"; }; &serdes_ln_ctrl { idle-states = <AM64_SERDES0_LANE0_PCIE0>; }; &serdes0 { serdes0_pcie_link: phy@0 { reg = <0>; cdns,num-lanes = <1>; #phy-cells = <0>; cdns,phy-type = <PHY_TYPE_PCIE>; resets = <&serdes_wiz0 1>; }; }; &pcie0_rc { status = "disabled"; }; &pcie0_ep { status = "disabled"; }; &tscadc0 { /* ADC is reserved for R5 usage */ status = "reserved"; }; &ospi0 { pinctrl-names = "default"; pinctrl-0 = <&ospi0_pins_default>; flash@0{ compatible = "jedec,spi-nor"; reg = <0x0>; spi-tx-bus-width = <8>; spi-rx-bus-width = <8>; spi-max-frequency = <25000000>; cdns,tshsl-ns = <60>; cdns,tsd2d-ns = <60>; cdns,tchsh-ns = <60>; cdns,tslch-ns = <60>; cdns,read-delay = <4>; cdns,phy-mode; #address-cells = <1>; #size-cells = <1>; }; }; &main_mcan0 { status = "disabled"; }; &main_mcan1 { status = "disabled"; }; &icssg0_mdio { pinctrl-names = "default"; pinctrl-0 = <&icssg0_mdio0_pins_default>; // reset-gpios = <&main_gpio1 25 GPIO_ACTIVE_LOW>,<&main_gpio1 5 GPIO_ACTIVE_LOW>; // reset-delay-us = <2>; /* PHY datasheet states 1uS min */ status = "okay"; icssg0_phy1: ethernet-phy@0 { reg = <0>; ti,tx-internal-delay = <DP83867_RGMIIDCTL_250_PS>; ti,rx-internal-delay = <DP83867_RGMIIDCTL_2_00_NS>; ti,fifo-depth = <DP83867_PHYCR_FIFO_DEPTH_4_B_NIB>; }; icssg0_phy2: ethernet-phy@1 { reg = <1>; ti,tx-internal-delay = <DP83867_RGMIIDCTL_250_PS>; ti,rx-internal-delay = <DP83867_RGMIIDCTL_2_00_NS>; ti,fifo-depth = <DP83867_PHYCR_FIFO_DEPTH_4_B_NIB>; }; }; /*&icssg0_iep0 { status = "okay"; // pinctrl-names = "default"; // pinctrl-0 = <&icssg0_iep0_pins_default>; };*/ &icssg1_mdio { status = "disabled"; };