Part Number: TDA4VM
Tool/software:
Dear TI
We made a new board based on TDA4VM board. And the connections between Ethernet device are like below.
| CPSW5G port 1 | -- RGMII -- | TI PHY(DP83867) |
| port 2 | -- RGMII -- | TI PHY(DP83867) |
| port 3 | -- RGMII -- | Marvell 8 port switch(88E6390 |
I'm using ti-processor-sdk-linux-j7200-evm-09_02_00_04, and the default manual mode setting of davinci MDIO is true.
When I tried to access registers of 88E6390, it returned all 0xFF.
So I changed manual mode to false and succeeded to read registers of 88E6390.
But it sometimes displayed below console log.
[ 424.996967] am65-cpsw-nuss c000000.ethernet eth0: Link is Down
[ 426.021393] am65-cpsw-nuss c000000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx
In our board, eth0 is port 1 which is connected with DP83867.
When I added debug code at int genphy_update_link(struct phy_device *phydev) function in phy_device.c, it sometimes read strange value from DP83867.
** read MII_BMCR instead of MII_BMSR
---------------------------------------------------------------------------------------------
[ 107.844410] ### genphy_update_link : 0x1140
[ 107.849906] am65-cpsw-nuss c000000.ethernet eth0: Link is Down
----------------------------------------------------------------------------------------------
** can not read valid register.
----------------------------------------------------------------------------------------------
[ 214.084127] ### genphy_update_link : 0x0
[ 214.089385] am65-cpsw-nuss c000000.ethernet eth0: Link is Down
----------------------------------------------------------------------------------------------
And it read valid register value(0x0x796d) next time and report Link up.
Could you give some advice how to debug this issue ?
FYI, this problem does not happen when I set manual mode to true. But 88E6390 is not accessible in setting manual mode to true.
BR
Jace