Part Number: AM625
Other Parts Discussed in Thread: UNIFLASH, SK-AM62-LP
Tool/software:
I want to write to OSPI using a custom AM625 board.
I am trying to run examples/drivers/ospi/ospi_flash_diag first because I cannot configure OSPI.
When I write using uart_bootloader.py, I get the following error.
[STATUS] ERROR: Application load FAILED !!!
Since I am using NT6AN256M16AC for DDR, I output the settings in syscfg and applied them to sbl_uart_uniflash.
Reference Design SK-AM62-LP with NT6AN256M16AC is used as is.
Are there any other areas that need to be configured?