Hi,
We have a system in which, AM3894 and Xilinx FPGA is present. Below is details of the system.
- AM3894 is configured as root complex
- AM3894 X1 lane is connected to FPGA and the unused lane of the AM3894 is unconnected or left open.
- Xilinx is 2.5Gts X1 lane End point
The system is inconsistent in detecting PCIe interface
We are able to see Xilinx Endpoint with LSPCI command on Linux. In the failure condition we have read LTSSM status bits. During link training failure LTSSM value is states Polling Compliance.
We are using the same software package as of 816x/389x EVM from Digital Spectrum.
Please can anyone suggest solution for this issue.
Regards,
SMK