This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM3730 gst Plugins TIVidenc1 bitRate Properties Invalid

Hi My dvsdk version is 4_02_00_06

set TIVidenc1 element properties bitRate=1500000 , pipeline work fine !

But use VLC to receive the MPEG-TS ,VLC report the bitRate > 1500000 bit/s ,some times the maxbitRate achieve to 3M bit/s

It seems TIVidenc1 bitRate Parameter is Invalid  ! Why ?

The following gst pipeline to test  .

gst-launch -e v4l2src always-copy=FALSE queue-size=4 ! 'video/x-raw-yuv,format= (fourcc)UYVY,width=720,height=576,framerate=(fraction)25/1' ! TIPrepEncBuf cont iguousInputFrame=TRUE numOutputBufs=4 ! queue max-size-buffers=4 max-size-byte s=0 ! TIVidenc1 codecName=h264enc engineName=codecServer bitRate=1500000 ! dma iperf ! mux. alsasrc ! audio/x-raw-int,rate=48000,channels=2 ! ffenc_mp2 bitrat e=64000 ! mux. mpegtsmux name=mux ! queue ! rtpmp2tpay ! udpsink port=8554 host =192.168.1.3

================================================================================================

Try set TIvidenc1 element properties rateControlPreset=2 (CBR),or encodingPreset =3 .

But gst pipeline can't work, TIVidenc1 has error! (failed to create video encoder: h264enc)

Use The following gst pipeline to test

=================================================================================================

gst-launch -e v4l2src always-copy=FALSE queue-size=4 ! 'video/x-raw-yuv,format= (fourcc)UYVY,width=720,height=576,framerate=(fraction)25/1' ! TIPrepEncBuf cont iguousInputFrame=TRUE numOutputBufs=4 ! queue max-size-buffers=4 max-size-byte s=0 ! TIVidenc1 bitRate=1500000 rateControlPreset=2 codecName=h264enc engineNa me=codecServer ! dmaiperf ! mux. alsasrc ! audio/x-raw-int,rate=48000,channels= 2 ! ffenc_mp2 bitrate=64000 ! mux. mpegtsmux name=mux ! queue ! rtpmp2tpay ! u dpsink port=8554 host=192.168.1.3

Setting pipeline to PAUSED ...

Pipeline is live and does not need PREROLL ...

WARNING: from element /GstPipeline:pipeline0/GstDmaiperf:dmaiperf0:

There is no codec present that can handle the stream's type. Additional debug info: gsttidmaiperf.c(285): gst_dmaiperf_start (): /GstPipeline:pipeline0/GstDmaiperf: dmaiperf0: Engine name not specified, not printing DSP information Setting pipeline to PLAYING ...

New clock: GstAudioSrcClock ERROR: from element /GstPipeline:pipeline0/GstTIVidenc1:tividenc10: failed to cr eate video encoder: h264enc

Additional debug info: gsttividenc1.c(1272): gst_tividenc1_codec_start (): /GstPipeline:pipeline0/GstTI Videnc1:tividenc10 Execution ended after 482940673 ns. Setting pipeline to PAUSED ...

Setting pipeline to READY ...

Setting pipeline to NULL ...

Freeing pipeline ...