This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-AM62A-LP: MCU Timer 0 clock configuration

Part Number: SK-AM62A-LP


Tool/software:

Hello, 

We are currently integrating an autosar stack on the MCU-R5F core of the SK-AM62A-LP board. Our autosar stack OS uses a systemticktimer mapped to the MCU_TIMER0 and is configured to 80MHz. The MCU_TIMER0 is using 25MHz as default and the HFOSC0_CLK as input clock.

I have the following questions -

1. We would like to know how do we configure the MCU_TIMER0 to 80MHz. Do we need a PLL config ? If yes. how exactly to configure it for exampe - which clock source, pll config methodoly and details etc

2. Once configured, how do we verify that the MCU_TIMER0 has been indeed set to 80MHz, for example- which system/core registers can be verified for this etc  

If you need further information, please feel free to ask 

Thanks and best regards,

Nikhil Bhat