Part Number: AM625SIP
Other Parts Discussed in Thread: AM625
Tool/software:
Hello, I am attempting to implement falcon mode on the AM625SIP in sdk10. I followed this forum e2e.ti.com/.../am625-how-to-setup-u-boot-falcon-boot-by-sdk-09_00_00_03
Here is my tispl.its file:
/dts-v1/;
/ {
description = "Configuration to load ATF and SPL";
#address-cells = <1>;
images {
atf {
description = "ARM Trusted Firmware";
data = /incbin/("/home/josiah/ti-processor-sdk-linux-am62xxsip-evm-10.00.07.04/board-support/prebuilt-images/am62xxsip-evm/bl31.bin");
type = "firmware";
arch = "arm64";
compression = "none";
os = "arm-trusted-firmware";
load = <0x9e780000>; /* This load/entry address pair is for use with AM62Ax */
entry = <0x9e780000>;
};
tee {
description = "OPTEE";
data = /incbin/("/home/josiah/ti-processor-sdk-linux-am62xxsip-evm-10.00.07.04/board-support/prebuilt-images/am62xxsip-evm/bl32.bin");
type = "tee";
arch = "arm64";
compression = "none";
os = "tee";
load = <0x9e800000>; /* Needs to match BL32_BASE in ATF */
entry = <0x9e800000>;
};
dm {
description = "DM binary";
data = /incbin/("/home/josiah/ti-processor-sdk-linux-am62xxsip-evm-10.00.07.04/board-support/prebuilt-images/am62xxsip-evm/ti-dm/am62xx/ipc_echo_testb_mcu1_0_release_strip.xer5f");
type = "firmware";
arch = "arm32";
compression = "none";
os = "DM";
load = <0x89000000>;
entry = <0x89000000>;
};
kernel {
description = "Linux Kernel (64-bit)";
data = /incbin/("/home/josiah/ti-processor-sdk-linux-am62xxsip-evm-10.00.07.04/board-support/built-images/Image");
type = "standalone";
os = "linux";
arch = "arm64";
compression = "none";
load = <0x80080000>; /* Needs to match PRELOADED_BL33_BASE in ATF */
entry = <0x80080000>;
};
fdt {
description = "k3-am625-sk";
data = /incbin/("/home/josiah/ti-processor-sdk-linux-am62xxsip-evm-10.00.07.04/board-support/built-images/dtb/ti/k3-am625-sk.dtb");
type = "flat_dt";
arch = "arm";
compression = "none";
load = <0x82000000>; /* Needs to match K3_HW_CONFIG_BASE in ATF */
};
};
configurations {
default = "k3-am625-sk";
k3-am625-sk {
description = "k3-am625-sk";
firmware = "atf";
loadables = "tee", "dm", "kernel", "fdt";
};
};
};Here is my patch of u-boot
From 81883f0b2230dc1b542152e41aa4aaea22a76138 Mon Sep 17 00:00:00 2001 From: Josiah Morrow <josiah_morrow@innovationfirst.com> Date: Fri, 25 Apr 2025 15:30:52 -0500 Subject: [PATCH] falcon mode 10.0 changes --- configs/am62x_evm_r5_defconfig | 5 +++-- include/configs/am62x_evm.h | 4 ++++ include/configs/ti_armv7_common.h | 16 ++++++++++++++++ include/env/ti/k3_dfu.h | 3 +-- 4 files changed, 24 insertions(+), 4 deletions(-) diff --git a/configs/am62x_evm_r5_defconfig b/configs/am62x_evm_r5_defconfig index 222765d0..61bbf9d4 100644 --- a/configs/am62x_evm_r5_defconfig +++ b/configs/am62x_evm_r5_defconfig @@ -1,5 +1,6 @@ CONFIG_ARM=y CONFIG_ARCH_K3=y +CONFIG_SYS_TEXT_BASE=0x83000000 CONFIG_SYS_MALLOC_LEN=0x08000000 CONFIG_SYS_MALLOC_F_LEN=0x9000 CONFIG_SPL_LIBCOMMON_SUPPORT=y @@ -20,7 +21,7 @@ CONFIG_DM_RESET=y CONFIG_SPL_MMC=y CONFIG_SPL_SERIAL=y CONFIG_SPL_DRIVERS_MISC=y -CONFIG_SPL_STACK_R_ADDR=0x82000000 +CONFIG_SPL_STACK_R_ADDR=0x89000000 CONFIG_SPL_SYS_MALLOC_F_LEN=0x7000 CONFIG_SPL_SIZE_LIMIT=0x3A7F0 CONFIG_SPL_SIZE_LIMIT_PROVIDE_STACK=0x3500 @@ -29,7 +30,7 @@ CONFIG_SPL_LIBDISK_SUPPORT=y CONFIG_SPL_SPI_FLASH_SUPPORT=y CONFIG_SPL_SPI=y CONFIG_SPL_LOAD_FIT=y -CONFIG_SPL_LOAD_FIT_ADDRESS=0x80080000 +CONFIG_SPL_LOAD_FIT_ADDRESS=0x84000000 # CONFIG_DISPLAY_CPUINFO is not set CONFIG_SPL_SIZE_LIMIT_SUBTRACT_GD=y CONFIG_SPL_SIZE_LIMIT_SUBTRACT_MALLOC=y diff --git a/include/configs/am62x_evm.h b/include/configs/am62x_evm.h index 6ef79d1b..cde92a91 100644 --- a/include/configs/am62x_evm.h +++ b/include/configs/am62x_evm.h @@ -28,4 +28,8 @@ #define CFG_SYS_NAND_ECCBYTES 14 /*-- end NAND config --*/ +#ifdef CONFIG_SYS_K3_SPL_ATF +#define CONFIG_SPL_FS_LOAD_PAYLOAD_NAME "tispl.bin" +#endif + #endif /* __CONFIG_AM625_EVM_H */ diff --git a/include/configs/ti_armv7_common.h b/include/configs/ti_armv7_common.h index 3def7b10..117678bd 100644 --- a/include/configs/ti_armv7_common.h +++ b/include/configs/ti_armv7_common.h @@ -31,6 +31,21 @@ * blob before loading the ramdisk, as DTBO location is only used as a temporary * storage, and can be re-used after 'fdt apply' command is done. */ +#if defined(CONFIG_CPU_V7R) && defined(CONFIG_SOC_K3_AM625) +#define DEFAULT_LINUX_BOOT_ENV \ + "loadaddr=0x84000000\0" \ + "kernel_addr_r=0x84000000\0" \ + "fdtaddr=0x88000000\0" \ + "dtboaddr=0x89000000\0" \ + "fdt_addr_r=0x88000000\0" \ + "fdtoverlay_addr_r=0x89000000\0" \ + "rdaddr=0x88080000\0" \ + "ramdisk_addr_r=0x88080000\0" \ + "scriptaddr=0x80000000\0" \ + "pxefile_addr_r=0x80100000\0" \ + "bootm_size=0x10000000\0" \ + "boot_fdt=try\0" +#else #define DEFAULT_LINUX_BOOT_ENV \ "loadaddr=0x82000000\0" \ "kernel_addr_r=0x82000000\0" \ @@ -44,6 +59,7 @@ "pxefile_addr_r=0x80100000\0" \ "bootm_size=0x10000000\0" \ "boot_fdt=try\0" +#endif #define DEFAULT_FIT_TI_ARGS \ "boot_fit=0\0" \ diff --git a/include/env/ti/k3_dfu.h b/include/env/ti/k3_dfu.h index 098f5f5d..2073d849 100644 --- a/include/env/ti/k3_dfu.h +++ b/include/env/ti/k3_dfu.h @@ -40,7 +40,6 @@ #define DFU_ALT_INFO_RAM \ "dfu_alt_info_ram=" \ - "tispl.bin ram 0x80080000 0x200000;" \ - "u-boot.img ram 0x81000000 0x400000\0" \ + "tispl.bin ram 0x84000000 0x4000000\0" #endif /* __TI_DFU_H */ -- 2.34.1
After loading the tiboot3.bin and tispl.bin I get the following boot log.U-Boot SPL 2024.04-dirty (Apr 25 2025 - 14:53:40 -0500)
SYSFW ABI: 4.0 (firmware rev 0x000a '10.0.8--v10.00.08 (Fiery Fox)')
SPL initial stack usage: 13392 bytes
Trying to boot from MMC1
Warning: Did not detect image signing certificate. Skipping authentication to prevent boot failure. This will fail on Security Enforcing(HS-SE) devices
Warning: Did not detect image signing certificate. Skipping authentication to prevent boot failure. This will fail on Security Enforcing(HS-SE) devices
Warning: Did not detect image signing certificate. Skipping authentication to prevent boot failure. This will fail on Security Enforcing(HS-SE) devices
fdt_fixup_memory_banks: FDT_ERR_BADMAGIC
Error fixing up memory node! -9
Warning: Did not detect image signing certificate. Skipping authentication to prevent boot failure. This will fail on Security Enforcing(HS-SE) devices
Warning: Did not detect image signing certificate. Skipping authentication to prevent boot failure. This will fail on Security Enforcing(HS-SE) devices
Starting ATF on ARM64 core...
NOTICE: BL31: v2.10.0(release):v2.10.0-367-g00f1ec6b87-dirty
NOTICE: BL31: Built : 16:09:05, Feb 9 2024
Any help that you could give me would be greatly appreciated.