This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM62A7: About the tuning steps of the DCC tool

Part Number: AM62A7


Tool/software:

Hi TI experts,


Should I execute each plugin in sequence, export the XML,

use the Imaging tool to generate a bin file,

flash it to the development board,

and then continue to execute the next plugin?

Best Regards,

Meng

  • Hi Meng,

    Even though you can tune multiple plugins and generate multiple XML files before generating the bin files, it is recommended to tune the plugin one by one. This way, you can test and verify the tuning effect of each plugin individually. 

    When you tune a certain plugin, for example, edge enhancement, you can use the live tuning feature which allows you to change the parameters and see the effect immediately without flashing the bin file to EVM.

    Regards,

    Jianzhong