This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VL-Q1: TDA4VL-Q1: Partial problem confirmation of WDG module in MCAL

Part Number: TDA4VL-Q1

Tool/software:

Hi team,

MCAL VERSION 10.1

There are several WDG module issues that need to be consulted.

1)Why call function Wdg_Trigger in function Wdg_SetTriggerCondition?

In this way, the condition indicated by the red box in the following image must be met

 These two functions should be called asynchronously?

2)Can it be configured to reset mode when the watchdog overflows? It seems that the EB tool does not allow it