Part Number: AM620-Q1
Tool/software:
In the description of ti, the MCU only mode of AM62X does not support configuring the MCU as a wake-up source in version 10.00.070.04. If so, how do we configure it

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM620-Q1
Tool/software:
In the description of ti, the MCU only mode of AM62X does not support configuring the MCU as a wake-up source in version 10.00.070.04. If so, how do we configure it

Hello,
Please see the Userspace command directly above where you circled.
In newer SDK, the qos_latency is the contrstraint sent to the DM firmware to determine which low power mode to enter.
Best Regards,
Anshu
Hello,
For more details about the latency constraint, see the TISCI documentation: https://downloads.ti.com/tisci/esd/latest/2_tisci_msgs/pm/lpm.html#tisci-msg-lpm-set-latency-constraint
The number written to this SYSFS entry will determine which low power mode to enter. 100 can be used for MCU Only mode.
Thanks,
Anshu
Hello,
I don't really understand how to configure the MCU ONLY in
Do I need to modify the code in the SDK of 11.00.09.04 to implement the MCU only function?
If you want to modify the source code of the SDK, please ask whether the SDK version 10.00.07.04 we use supports modifying the source code to implement MCU ONLY
Hello,
As stated in the Linux SDK documentation, the only command before suspending is
echo 100 > /sys/devices/system/cpu/cpu0/power/pm_qos_resume_latency_us
There are no other changes required.
Thanks,
Anshu