This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux: "Empty flash at..." -- a problem?

Other Parts Discussed in Thread: OMAP3530

Hello, everyone.

I'm working on a custom OMAP3530 board and trying to make Linux boot and run from NAND flash.

Linux does, but during the boot process I get a bunch of messages:

[    3.793853] Empty flash at 0x0000fffc ends at 0x00010000
[    3.816162] Empty flash at 0x0002fffc ends at 0x00030000

.... And so on.

So I have two questions:

1. What causes these messages?

2. Is this a problem to fix or something tolerable to live with (because Linux is running)?

 

Details:

NAND Chip: Micron's MT29F8G16ADBDAH4

U-boot reports: Device 0: NAND 1GiB 1,8V 16-bit, sector size 128 KiB

U-boot and Kernel sources are derived from Arago hosted PSP_04.02.00.07

NAND contains an JFFS2 image, built and flashed from u-boot in accordance with PSP_04.02.00.07 User Guide.

 

Thanks.