Other Parts Discussed in Thread: DM3730
Hi,
I've got a problem to run the remotefx demo with beagle-xm.
The server is based on AMD Phenom II X955 and FirePro V8800.
OSs: Windows Server 2008 R2 SP1 the host,
Windows 7 SP1 32bit the hyper-V based vdi.
Test from another Windows 7 machine, everything is very good.
But when i connect the vdi through beagle-xm, the client is so calm to do nothing.
After a hard work. Find that it is caused by the non-synced time between VDI and the beagle-xm.
Just have the time synced. Now I can see the welcome screen of the VDI. But just the welcome, nothing else.
It stops there.
Any idea to fix it?
The log from the serial console is as below.
MPC Data Compact 7 SD X-Loader for BeagleBoard xM3730
Built Nov 2 2010 at 18:20:39
Version BSP_WEC7_ARM_A8 2.00.00.12
open ebootsd.nb0 file
Init HW: controller RST
SDCARD: reqested speed 1000000, actual speed 1000000
SDCARD: reqested speed 25000000, actual speed 19200000
ݹ™¥ÕÉM•==Q™½É…]•…Ý}I5}áɹÁÁ¹ÁÁ¹ÅÉ5)5)Q%=5AÑÕ…±ÍÁ••‘ÅÁÁÁÁÁÁ5)ÿSDCARD: reqested speed 25000000, actual speed 19200000ÁÁÁÁÁ±…É‘½Ý¹±½…‘¹¹¹5)%9=éAÉ•‘½Ý¹±½…‘¹¹¹¹5)]IBLSDCardReadLogo: cannot open Logo.bmp
disable_lcd_backlight-
>>> Forcing cold boot (non-persistent registry and other data will be wiped) <<<
Hit space to enter configuration menu 5...
Hit space to enter configuration menu 4...
Hit space to enter configuration menu 3...
Hit space to enter configuration menu 2...
Hit space to enter configuration menu 1...
BL_IMAGE_TYPE_BIN
+OEMMultiBinNotify(0x87eb1e78 -> 1)
Download file information:
-----------------------------------------------------------
[0]: Address=0x80002000 Length=0x022d74e0 Save=0x80002000
-----------------------------------------------------------
Download file type: 1
-OEMMultiBinNotify
+OEMIsFlashAddr(0x80002000)
-OEMIsFlashAddr(rc = 0)
rom_offset=0x0.
ImageStart = 0x80002000, ImageLength = 0x22d74e0, LaunchAddr = 0x8000f840
Completed file(s):
-------------------------------------------------------------------------------
+OEMIsFlashAddr(0x80002000)
-OEMIsFlashAddr(rc = 0)
[0]: Address=0x80002000 Length=0x22d74e0 Name="" Target=RAM
ROMHDR at Address 80002044h
+OEMLaunch(0x80002000, 0x022d74e0, 0x8000f840, 0x822d685c - 4/1)
Launch Windows CE image by jumping to 0x8000f840...
Windows CE Kernel for ARM (Thumb Enabled)
INFO:OALLogSetZones: dpCurSettings.ulZoneMask: 0x800b
OAL: CPU revision 0x10:DM3730
OAL: CPU L2 Aux register 0x400042
****Profiler Build****
---High Performance Frequency is 32768 hz---
PID:00400002 TID:00410002 opm0: chipOffOffset:10161,332 chipOSWROffset:799,26 chipCSWROffset:633,20 coreCSWROffset:379,12 coreInactiveOffset:379,12 mpuInactiveOffset:379,12
PID:00400002 TID:00410002 opm1: chipOffOffset:9916,324 chipOSWROffset:755,24 chipCSWROffset:633,20 coreCSWROffset:379,12 coreInactiveOffset:379,12 mpuInactiveOffset:379,12
PID:00400002 TID:00410002 opm2: chipOffOffset:8024,262 chipOSWROffset:725,23 chipCSWROffset:633,20 coreCSWROffset:379,12 coreInactiveOffset:379,12 mpuInactiveOffset:379,12
PID:00400002 TID:00410002 opm3: chipOffOffset:8024,262 chipOSWROffset:694,22 chipCSWROffset:633,20 coreCSWROffset:379,12 coreInactiveOffset:379,12 mpuInactiveOffset:379,12
PID:00400002 TID:00410002 opm4: chipOffOffset:8024,262 chipOSWROffset:694,22 chipCSWROffset:633,20 coreCSWROffset:379,12 coreInactiveOffset:379,12 mpuInactiveOffset:379,12
PID:00400002 TID:00410002 opm5: chipOffOffset:8024,262 chipOSWROffset:694,22 chipCSWROffset:633,20 coreCSWROffset:379,12 coreInactiveOffset:379,12 mpuInactiveOffset:379,12
PID:00400002 TID:00410002 opm6: chipOffOffset:8024,262 chipOSWROffset:694,22 chipCSWROffset:633,20 coreCSWROffset:379,12 coreInactiveOffset:379,12 mpuInactiveOffset:379,12
PID:00400002 TID:00870006 SDHC: CPU revision 0x10
PID:00400002 TID:00870006 SDHC host controller initialize: m_fastPathSDIO:1 m_fastPathSDMEM:0
PID:00400002 TID:00870006 +UBD_Init(Drivers\Active\24, 0x00000000)
PID:00400002 TID:00870006 UBD_Init: PinMode (0x00000003)
PID:00400002 TID:00870006 UBD_Init: SysIntr (0x00000015)
PID:00400002 TID:00870006 -UBD_Init(rc = -1002034928)
PID:00400002 TID:00870006 ULPI VID Low 0x24
PID:00400002 TID:00870006 ULPI VID High 0x4
PID:00400002 TID:00870006 ULPI PID Low 0x7
PID:00400002 TID:00870006 ULPI PID High 0x0
PID:00400002 TID:00870006 ULPI Function 0x45
PID:00400002 TID:00870006 ULPI Interface 0x18
PID:00400002 TID:00870006 ULPI OTG 0x66
PID:00400002 TID:00870006 ULPI USB IO PM 0x4
PID:00400002 TID:00870006 UfnClientLib!UfnCheckPID: WARNING -- using MS reference platform VID/PID 0x045e/0x00ce (not allowed in shipping platforms)
PID:00400002 TID:00870006 DSPLINK Module (1.65.00.03) created on Date: Oct 27 2010 Time: 15:50:00
PID:00400002 TID:01C40012 KeybdDriverInitializeEx: Layout Manager successfully initialized to 1
PID:00400002 TID:01C40012 LayoutMgrActivateKeyboardLayout: Called with hkl = 0x00000409
PID:00A0000E TID:03D8005E MSIM: IM_ReadRegistry read KB 5
PID:032A001E TID:03370062 Explorer(V2.0) taskbar thread started.
PID:00400002 TID:02D90066 SMSC: LAN9500 USB 2.0 to Ethernet 10/100 Driver.
PID:00400002 TID:02D90066 SMSC: DRIVER_VERSION : V1.10.0001.0000
PID:00400002 TID:02D90066 SMSC: DATECODE : 051209
PID:00400002 TID:02D90066 SMSC: Built on Nov 4 2010 at 14:35:50
PID:00400002 TID:00CB0006 kernel IOCTL_POWER_SET setting state 1
PID:00400002 TID:00CB0006 kernel IOCTL_POWER_SET setting state 0
PID:040C001A TID:054E001E CTLPNL: cmdline=clock.cpl
PID:040C001A TID:054E001E --->>>CTLPNL: CPL='clock.cpl' icon=0 tab=0
PID:00400002 TID:00CB0006 kernel IOCTL_POWER_SET setting state 1
PID:00400002 TID:00CB0006 kernel IOCTL_POWER_SET setting state 0
PID:00D203FE TID:054C003A ### Trace initialized (d203fe:54c003a) at 18:42:36.00 05/12/2011 ###
PID:00D203FE TID:054C003A ### Loading symbols (d203fe:54c003a) at 18:42:36.00 05/12/2011 ###
PID:00D203FE TID:054C003A ### Symbols loaded (d203fe:54c003a) at 18:42:36.00 05/12/2011 ###
PID:00D203FE TID:059D004A Exception 'Raised Exception' (0x6ba): Thread-Id=059d004a(pth=c0441bd8), Proc-Id=00d203fe(pprc=c0485c98) 'cetsc.exe', VM-active=00d203fe(pprc=c0485c98) 'cetsc.exe'
PID:00D203FE TID:059D004A PC=40029dd0(coredll.dll+0x00019dd0) RA=800362cc(kernel.dll+0x0000e2cc) SP=0028f10c, BVA=00000000
PID:00D203FE TID:059D004A 18:42:37.00!d203fe:59d004a!CDynVCPlugin!1447!Expression failed: spSurfBinding
PID:00D203FE TID:059D004A 18:42:37.00*d203fe:59d004a*CDynVCPlugin*1449*Failed to retrieve surface manager interface. hr[0x80004005]
PID:00400002 TID:04720062 DSP Clk Rate 800000
PID:00D203FE TID:04A5004E Exception 'Data Abort' (0x4): Thread-Id=04a5004e(pth=c045f488), Proc-Id=00d203fe(pprc=c0485c98) 'cetsc.exe', VM-active=00d203fe(pprc=c0485c98) 'cetsc.exe'
PID:00D203FE TID:04A5004E PC=4177d91c(mstscax.dll+0x000ad91c) RA=00000001(???+0x00000001) SP=0032fb9c, BVA=00ab002a
PID:00400002 TID:04A5004E Exception 'Raised Exception' (0x116): Thread-Id=04a5004e(pth=c045f488), Proc-Id=00400002(pprc=822f25e0) 'NK.EXE', VM-active=00d203fe(pprc=c0485c98) 'cetsc.exe'
PID:00400002 TID:04A5004E PC=eff6d638(k.coredll.dll+0x0001d638) RA=800362cc(kernel.dll+0x0000e2cc) SP=d17ff3b4, BVA=ffffffff
PID:00D203FE TID:04A5004E Exception 'Data Abort' (0x4): Thread-Id=04a5004e(pth=c045f488), Proc-Id=00d203fe(pprc=c0485c98) 'cetsc.exe', VM-active=00d203fe(pprc=c0485c98) 'cetsc.exe'
PID:00D203FE TID:04A5004E PC=4177d91c(mstscax.dll+0x000ad91c) RA=00000001(???+0x00000001) SP=0032fb9c, BVA=0078002a
PID:00400002 TID:04A5004E Exception 'Raised Exception' (0x116): Thread-Id=04a5004e(pth=c045f488), Proc-Id=00400002(pprc=822f25e0) 'NK.EXE', VM-active=00d203fe(pprc=c0485c98) 'cetsc.exe'
PID:00400002 TID:04A5004E PC=eff6d638(k.coredll.dll+0x0001d638) RA=800362cc(kernel.dll+0x0000e2cc) SP=d17ff3b4, BVA=ffffffff
PID:00D203FE TID:059D004A 18:42:40.00*d203fe:59d004a*CDynVCPlugin*1974*Can't find listener "PNPDR"
PID:00D203FE TID:059D004A 18:42:40.00*d203fe:59d004a*CDynVCPlugin*1974*Can't find listener "URBDRC"
PID:00400002 TID:00CB0006 kernel IOCTL_POWER_SET setting state 1
PID:00400002 TID:00CB0006 kernel IOCTL_POWER_SET setting state 2
PID:00D203FE TID:054C003A ERROR: this platform does not support BlurEffect.PID:00D203FE TID:054C003A ERROR: this platform does not support DropShadowEffect.PID:00D203FE TID:054C003A ERROR: this platform does not support RippleEffect.PID:00D203FE TID:054C003A ERROR: eglGetDisplay() failed with error 0x3000PID:00D203FE TID:054C003A ERROR: COpenGLDevice::Initialize(), hr = 0x80004005PID:00D203FE TID:054C003A ERROR: eglGetDisplay() failed with error 0x3000PID:00D203FE TID:054C003A ERROR: COpenGLDevice::Initialize(), hr = 0x80004005PID:00D203FE TID:054C003A ERROR: eglGetDisplay() failed with error 0x3000PID:00D203FE TID:054C003A ERROR: COpenGLDevice::Initialize(), hr = 0x80004005PID:00D203FE TID:054C003A ERROR: eglGetDisplay() failed with error 0x3000PID:00D203FE TID:054C003A ERROR: COpenGLDevice::Initialize(), hr = 0x80004005PID:00D203FE TID:054C003A ERROR: eglGetDisplay() failed with error 0x3000PID:00D203FE TID:054C003A ERROR: COpenGLDevice::Initialize(), hr = 0x80004005PID:00D203FE TID:054C003A ERROR: eglGetDisplay() failed with error 0x3000PID:00D203FE TID:054C003A ERROR: COpenGLDevice::Initialize(), hr = 0x80004005PID:00D203FE TID:054C003A ERROR: eglGetDisplay() failed with error 0x3000PID:00D203FE TID:054C003A ERROR: COpenGLDevice::Initialize(), hr = 0x80004005PID:00D203FE TID:054C003A ERROR: eglGetDisplay() failed with error 0x3000PID:00D203FE TID:054C003A ERROR: COpenGLDevice::Initialize(), hr = 0x80004005PID:00D203FE TID:054C003A ERROR: eglGetDisplay() failed with error 0x3000PID:00D203FE TID:054C003A ERROR: COpenGLDevice::Initialize(), hr = 0x80004005PID:00D203FE TID:054C003A ERROR: eglGetDisplay() failed with error 0x3000PID:00D203FE TID:054C003A ERROR: COpenGLDevice::Initialize(), hr = 0x80004005PID:00D203FE TID:054C003A ERROR: eglGetDisplay() failed with error 0x3000PID:00D203FE TID:054C003A ERROR: COpenGLDevice::Initialize(), hr = 0x80004005PID:00D203FE TID:054C003A ERROR: eglGetDisplay() failed with error 0x3000PID:00D203FE TID:054C003A ERROR: COpenGLDevice::Initialize(), hr = 0x80004005PID:00D203FE TID:054C003A ERROR: eglGetDisplay() failed with error 0x3000PID:00D203FE TID:054C003A ERROR: COpenGLDevice::Initialize(), hr = 0x80004005PID:00D203FE TID:054C003A ERROR: eglGetDisplay() failed with error 0x3000PID:00D203FE TID:054C003A ERROR: COpenGLDevice::Initialize(), hr = 0x80004005PID:00D203FE TID:054C003A ERROR: eglGetDisplay() failed with error 0x3000PID:00D203FE TID:054C003A ERROR: COpenGLDevice::Initialize(), hr = 0x80004005PID:00D203FE TID:054C003A ERROR: eglGetDisplay() failed with error 0x3000PID:00D203FE TID:054C003A ERROR: COpenGLDevice::Initialize(), hr = 0x80004005PID:00D203FE TID:054C003A ERROR: eglGetDisplay() failed with error 0x3000PID:00D203FE TID:054C003A ERROR: COpenGLDevice::Initialize(), hr = 0x80004005PID:00D203FE TID:054C003A ERROR: eglGetDisplay() failed with error 0x3000PID:00D203FE TID:054C003A ERROR: COpenGLDevice::Initialize(), hr = 0x80004005PID:00D203FE TID:054C003A ERROR: eglGetDisplay() failed with error 0x3000PID:00D203FE TID:054C003A ERROR: COpenGLDevice::Initialize(), hr = 0x80004005PID:00D203FE TID:054C003A ERROR: eglGetDisplay() failed with error 0x3000PID:00D203FE TID:054C003A ERROR: COpenGLDevice::Initialize(), hr = 0x80004005PID:00D203FE TID:054C003A ERROR: eglGetDisplay() failed with error 0x3000PID:00D203FE TID:054C003A ERROR: COpenGLDevice::Initialize(), hr = 0x80004005PID:00D203FE TID:054C003A ERROR: eglGetDisplay() failed with error 0x3000PID:00D203FE TID:054C003A ERROR: COpenGLDevice::Initialize(), hr = 0x80004005PID:00D203FE TID:054C003A ERROR: eglGetDisplay() failed with error 0x3000PID:00D203FE TID:054C003A ERROR: COpenGLDevice::Initialize(), hr = 0x80004005PID:00D203FE TID:054C003A ERROR: eglGetDisplay() failed with error 0x3000PID:00D203FE TID:054C003A ERROR: COpenGLDevice::Initialize(), hr = 0x80004005PID:00D203FE TID:054C003A ERROR: eglGetDisplay() failed with error 0x3000PID:00D203FE TID:054C003A ERROR: COpenGLDevice::Initialize(), hr = 0x80004005
David Chan
Tongfang Co,. Ltd.