This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320DM648: Inquiry on replacement due to discontinuation of TMS320DM648ZUTA8

Guru 11130 points
Part Number: TMS320DM648

Tool/software:

Hello,

My customer has a few questions about the replacement of TMS320DM648CUTA8 due to discontinuation of TMS320DM648ZUTA8.

Q1. Are there any differences between these two products in terms of packaging, pin map, performance, S/W coding, etc.?

Q2. Are there any modifications that users should consider in advance when changing to TMS320DM648CUTA8 on a board that is already in production?

Q3. They execute the conversion to BOOTMODE via the pin settings below. Would it be okay to control it in the same way?

DIP SWITCH PIN

DIP SWITCH ON(1)/OFF(0)

DSP Matching PIN

1

0

AEA11_BOOTMODE0

2

0

AEA12_BOOTMODE1

3

1

AEA13_BOOTMODE2

4

0

AEA14_BOOTMODE3

5

0

AEA15_LENDIAN

6

1

AECLKINSEL/AEA17

7

0

AEA19

8

1

AEA20_DVREN

9

1

AEA21_FASTBOOT

10

1

AEA22_EMIFAWIDTH

Thank you.

JH