Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hi,
We get a problem that SPI signal not looks good, as show in the picture, it have a long tail on every frame data.
Am62A work as master with PIO mode,
Here is our config:
spi0_pins_default: spi0-default-pins {
pinctrl-single,pins = <
AM62AX_IOPAD(0x1b4, PIN_OUTPUT, 0) /* (D16) SPI0_CS0 - SOC_SPI0_nCS0 */
AM62AX_IOPAD(0x1bc, PIN_INPUT, 0) /* (A17) SPI0_CLK - SOC_SPI0_CLK */
AM62AX_IOPAD(0x1c0, PIN_OUTPUT, 0) /* (B15) SPI0_D0 - SOC_SPI0_MOSI */
AM62AX_IOPAD(0x1c4, PIN_INPUT, 0) /* (E15) SPI0_D1 - SOC_SPI0_MISO */
>;
};
&main_spi0 { status = "okay"; pinctrl-names = "default"; pinctrl-0 = <&spi0_pins_default>; ti,pindir-d0-out-d1-in; // set SPI0_D0: MOSI, SPI0_D1: MISO, default: d0-in-d1-out(SPI0_D0: MISO, SPI0_D1: MOSI) mcu-connector@0 { compatible = "ti,spi-mcu"; reg = <0>; spi-max-frequency = <5000000>; }; };