[FAQ] AM62L ( AM62L32 , AM62L31 ) Design Recommendations / Custom board hardware design - Processor Reset inputs, Reset Status Output and Connection recommendations

Part Number: AM62L
Other Parts Discussed in Thread: AM625

Tool/software:

HI TI experts,

I have queries related to supported reset inputs and reset status outputs 

Supported Reset inputs 

Recommended connections for Reset inputs 

Supported Reset Status output(s)

Recommended connections for Reset Status outputs

  • HI Board designers, 

    Please refer below.

    Supported Reset input and output signals

    Connection recommendations 

    Recommendations when RTC mode is used

    Sequencing of VDDS_RTC and VDD_RTC
    VDDS_RTC and VDD_RTC needs to be powered before RTC_PORz is released

    There is no sequencing requirement between VDDS_RTC and VDD_RTC.

    The only firm sequencing requirement for the AM62Lx processor is VDD_RTC up before and down after VDD_CORE.

    RTC_PORz delay when RTC mode is configured
    The RTC_PORz provides an asynchronous reset to the RTC domain and puts the logic is a known locked state until the VDD_CORE ramps. The LF oscillator is turned off by default. Once VDD_CORE ramps the RTC domain will partially unlock and start receiving its clock from the RC oscillator until software completes the unlock process by configuring the RTC domain. There is a glitch-free clock multiplexer that can be reconfigured from its default RC oscillator to select the LF oscillators after software has turned on the LF oscillator and waited 100ms for it to start. The max startup time for the LF oscillator with a crystal circuit is 98ms.

    Based on the above operation the customer only needs to ensure the VDD_RTC and VDDS_RTC power rails are valid before they release RTC_PORz.


    RC is used for RTC_PORz
    We do not recommend an RC generated reset because the signal rising slew rate is too slow to get a glitch free reset inside the device.


    SK RTC Only mode power supply architecture - a diode added to the VDD_RTC supply. Not sure on the use case
    VDD_RTC needs to ramp up before VDD_CORE and down after VDD_CORE. Without the diode the VDD_RTC power rail could decay at the same time or before VDD_CORE when there is a uncontrolled power down, where the system power supply is turned off or disconnected from the board. The VDD_RTC power domain doesn’t draw much power, so the input capacitors on the VDD_RTC LDO will hold the VDD_RTC rail valid for a long time when it is isolated from the input power supply with the diode.
    If there is a short interruption, the VDD_RTC supply may not decay to less than 0.3V before next power-up and I suspect this is not a concern.
    We do not expect a problem for this use case because the VDD_RTC power rail is expected to be one of the first power rails to turn on and the last to turn off. Plus the VDDS_RTC LDO will assert RTC_PORz as its output begins to decay and will also assert it again as its input begins to ramp after the short interruption.


    32K LFOSC0 clock when RTC mode is not used
    Can you please confirm if the 32K crystal can be a DNI and customer can follow the data sheet recommendation to connect Xi to ground when low power modes are not used?
    The low-frequency oscillator is not required to be connected when none of the RTC low power modes are being used. Follow the processor connection recommendation when LFOSC0 is not used.

    Recommendations when RTC or low power modes are not used
    Customer does not use low power modes. Is there a recommended connection for VDD_RTC, VDDS_RTC and RTC_PORz

    In the case where no low power mode is used:
    VDD_RTC is connected to the same 0.75V power supply that is powering VDD_CORE.
    VDDS_RTC is connected to the same 1.8V power supply that is powering VDDS_OSC0.
    RTC_PORz is connected to the same reset source that is sourcing PORz

    On the AM62L, PORz is 3.3V tolerant.
    Wanted to check id the RTC_PORz is also 3.3V tolerant. Based on the data sheet I do not see the RTC_PORz being 3.3V tolerant.
    The use case for the query is when RTC only or RTC + IO + DDR mode is not used, we are recommending connecting the input connected to PORz to be connected to RTC_PORz.


    PORz is the only 3.3V tolerant pin. The RTC_PORz pin is not 3.3V tolerant.

    In this case, the signal sourcing these two pins will need to be sourced from the same IO power supply that is sourcing VDDS_RTC because the voltage applied to the RTC_PORz pin needs to track VDDS_RTC since it is limited to the range of -0.3V to (VDDS_RTC IO supply voltage + 0.3V).

    The PORZ pin is powered from VDDS_OSC0, but it is okay for it to be sourced from VDDS_RTC since it is fail-safe. In the case you describe, I would expect VDDS_RTC and VDDS_OSC0 to be sourced from the same 1.8V power supply. However, I’m not aware of any problem if there is a system requirement to source VDDS_OSC0 from a different 1.8V supply than the one used to source VDDS_RTC.

    Regards,

    Sreenivasa

  • Hi Board designers,

    (+) [FAQ] AM625 / AM623 / AM620-Q1 / AM625-Q1 / AM625SIP: MCU_PORz input slew rate - Processors forum - Processors - TI E2E support forums

    Usually add RC filter on RESET signal to anti noise, but the slew rate requirement of RESET signal on AM62x datasheet is quite sharp, on customer board it is about 10V-100V/ms, can it meet AM62x reset requirement, if not please help to explain the basic mechanism. 

    There can be long-term reliability issues associate with the input buffer if the applied signal spends too much time in the voltage region between VIHSS and VILSS. The maximum transition time allowed is 1000ns. I recommend driving the reset input with a push-pull buffer that produces a signal transition rate that is faster than 5ns to eliminate the risk of noise coupling into the signal as it transitions through the input buffer switching threshold.

    A 22 pF glitch filter is recommended at the input of MCU_PORz

     another important point about the MCU_PORz input slew rate. It is very easy for noise to couple on slow rising signals such that it creates non-monotonic transitions. Your MCU_PORz reset source needs to be monotonic to prevent the chance of creating glitches on internal reset as it transitions through the input buffer switching threshold. A faster slew rate on the MCU_PORz will increase your system noise immunity. The min slew rate defined in the AM625 datasheet is acceptable to the AM625 device but may not be acceptable for your system noise immunity requirements.

    Please keep in mind the AM62x device requires the MCU_PORz input to have a maximum rise/fall time of 1000ns. This may be difficult to achieve with a pull-up on a signal sourced from an open-drain output buffer. You may need to buffer the open-drain signal with a push-pull buffer that has hysteresis on its input to ensure the AM62x device never receives a short reset pulse that violates the minimum pulse duration defined in the "MCU_PORz Timing Requirements" table. For example, it may be possible for noise to couple on the slow rising open-drain signal just as it crosses the input buffer threshold which could cause a short glitch on the reset signal. Normal device operation could be compromised if this occurs.

    See the "Input Slew Rate" parameter in the "Fail-Safe Reset (FS RESET) Electrical Characteristics" table.

    The MCU_PORz input is the only input on the AM62x device that is fail-safe and 3.3v tolerant. Therefore, you can pull the MCU_PORz signal to 1.8V or 3.3V.

    See the "Steady-state max voltage at all fail-safe IO pins" parameter for MCU_PORz in the "Absolute Maximum Ratings" table.

    Note: The MCU_PORz description above is valid for the AM62L PORz cold reset input.

    Regards,

    Sreenivasa