This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM62P: AM62P DSS display pipeline

Part Number: AM62P


Tool/software:

Hi Expert,

From Datasheet, we can see AM62P have 4 pipeline in total, but there is some limitation for pipeline.

Four display pipelines with hardware overlay support. A maximum of two display pipelines
may be used per display.

I want to double check with you about the 4 pipeline in on display, can you tell me is this feasible? What are the specific reasons why it is not feasible?

BR,

Biao 

  • Biao,
    AM62P has 2x DSS, each with 2 display pipelines (VID and VIDL), making total 4 as stated.

    Each DSS also has 2 Video Ports (VP) each, which can use these pipelines (present in the same DSS) individually or overlayed (meaning each VP can only get overlay from maximum 2 pipelines which are present in the same DSS). We currently only support one display panel per VP, hence the limitation: any display panel can be fed from maximum 2 display pipelines.