This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: Errors while using C++ libraries <string> and <istream> on CCS

Part Number: TDA4VM

Tool/software:

Hello TI, 

I'm using several C++ libraires as <string>, <ftsream>, <istream> on my project. 
In short, these libraries are used to download data from a file into the code.
During the compilation of the project, there is no single error.

However, whenever I try to launch a debug session, the algorithm remains in an infinite loop. I've tried debugging step by step, and here are the error messages I get:
- Can't find a source file at "e:\cvs\jenkins\workspace\buildandvalidate_worker\build\c70\product\pc\lib-internal\src/libcxx\string" 
- Can't find a source file at "e:\cvs\jenkins\workspace\buildandvalidate_worker\build\c70\product\pc\lib-internal\src/libcxx\istream" 

I don't understand those errors messages...

Thank you all, 
Mélanie