This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6442: PRU to R5F Host Interrupt Performace

Part Number: AM6442

Tool/software:

My thread is locked without an answer, so I need to open a new one.

Please refer to the original thread for the issue's details.

Thanks.

  • Tushar Thakur, would it be possible for you to reassign an expert to this issue, or should I conclude that it's unsolvable?

    Many thanks

  • Hi Francesco,

    From the above link, I can see there are three questions pending.

    1. How much is the typical api/soc delay introduced by GPIO_pinWriteHigh?

    2. How much is the latency of VIM / HwiP_* api?

    3. What interrupt handling resources are shared between R5 cores?

    Please confirm the above for better assistance.

    Regards,

    Tushar

  • Yes, plus,

    4. Can I implement any configuration to have a more deterministic delay?

    Thanks!

  • Hello Franceso,

    one information I couldn't find in your other post is where your code is executing from. Did you try putting all of your R5f code into TCM?

    If your code is located in MSRAM or even worse in DDR memory there are rather huge latencies when code isn't available in the L1 cache, and that cache is rather small and from my experience often misses. Of course this depends on the whole code executing on that R5f core at the time.

    If you manage to put all of your code into TCM you eliminate that factor.

    On a scale of a few hundred ns that could be relevant.

    Please note that I'm not TI, and they may have other advice for you.

    Regards,

    Dominic

  • Ciao Dominic,

    thanks for the hints, unfortunately the code is already executed from TCMA and TCMB the data/memory segments are on MSRAM in other to be shared with PRU.

    Francesco.

  • Hi Francesco,

    Thanks for your patience.

    1. How much is the typical api/soc delay introduced by GPIO_pinWriteHigh?

    The average cycle taken to make GPIO pin high is ~160 cycles from R5F running at 800 MHz.

    2. How much is the latency of VIM / HwiP_* api?

    The average time taken to call the user callback function once the ISR is generated is ~365 cycles from R5F running at 800 MHz.

    All the above results are taken from release build of the provided project.

    Please refer below project.

    Project - interrupt_latency_am64x-evm_r5fss0-0_nortos_ti-arm-clang.zip

    3. What interrupt handling resources are shared between R5 cores?

    Please refer section 6.2.3.1 R5FSS Block Diagram of device TRM for this information.

    Can I implement any configuration to have a more deterministic delay?

    You can use the above program to calculate benchmarking number and have more deterministic way of getting interrupts.

    Regards,

    Tushar