This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM62L-PROCESSOR-SDK: Error Prints from TISPL.

Part Number: AM62L-PROCESSOR-SDK


Tool/software:

Hello,

I have updated some of the changes which requires for a proper booting of the customised board with 1GB DDR. And the board boots proerly till user space. But i found some error prints which are attached below.Does it effect the Board, How to overcome those error prints.

 reboot: Restarting system
NOTICE:  bl1_plat_arch_setup arch setup 
NOTICE:  Booting Trusted Firmware
NOTICE:  BL1: v2.12.0(release):a36507324-dirty
NOTICE:  BL1: Built : 05:35:22, Apr 29 2025
NOTICE:  lpdd4_init <-- 
NOTICE:  DDR ram size =40000000 
NOTICE:  bl1_platform_setup DDR init done
NOTICE:  k3_bl1_handoff ENTERING WFI - end of bl1
NOTICE:  BL31: v2.12.0(release):a36507324-dirty
NOTICE:  BL31: Built : 05:35:22, Apr 29 2025
ERROR:   Failed to get response (-19)
ERROR:   Transfer send failed (-19)
ERROR:   Agent 0 Protocol 0x10 Message 0x7: not supported

U-Boot SPL 2025.01-ge92ebf9f7bcb (Apr 28 2025 - 11:07:19 +0000)
SPL initial stack usage: 1744 bytes
Trying to boot from MMC2
ERROR:   Agent 0 Protocol 0x10 Message 0x7: not supported


U-Boot 2025.01-ge92ebf9f7bcb (Apr 28 2025 - 11:07:19 +0000)

SoC:   AM62LX SR1.0 HS-FS
Model: iG-RainboW-G69M-TI-AM62LX OSM
DRAM:  1 GiB
ERROR:   Agent 0 Protocol 0x10 Message 0x7: not supported
Core:  59 devices, 27 uclasses, devicetree: separate
MMC:   mmc@fa10000: 0, mmc@fa00000: 1
Loading Environment from nowhere... OK
In:    serial@2800000
Out:   serial@2800000
Err:   serial@2800000

Board Info:
        BSP Version               : iG-PRITZ-SC-01-R1.0-REL0.1-Linux6.12.13
        SOM Version               : iG-PRITZ-AP-01-R1.0
Net:   ADIN1300 PHY detected at addr 4

Warning: ethernet@8000000port@1 MAC addresses don't match:
Address in ROM is               44:6b:1f:35:33:54
Address in environment is       a0:cd:f3:77:ef:49
eth0: ethernet@8000000port@1 [PRIME]
Hit any key to stop autoboot:  0 


ERROR: Failed to get response (-19)
ERROR: Transfer send failed (-19)
ERROR: Agent 0 Protocol 0x10 Message 0x7: not supported

--Regards,
Dheeraj k