Tool/software:
Here's a complete, clearly documented technical support note that you can share with TI Customer Support. This will help them understand your exact process, image, and problem so they can guide you properly.
Board:
-
TI SoC: AM68A
-
Board Platform: j721s2-evm (AM68A is based on this SoC)
Steps I Followed
1. SDK Configuration Used
I used the following SDK configuration:
-
SDK:
processor-sdk-analytics-10.01.00 -
Config file:
processor-sdk-analytics-10.01.00-config.txt
Targeted for AM68A (j721s2-evm)
2. ️ Yocto Build
I built the full image using Yocto:
MACHINE=j721s2-evm bitbake tisdk-edgeai-image
The build completed successfully.
3. Image Obtained
After build, I got the following image:
-
Image:
tisdk-edgeai-image-j721s2-evm.rootfs-20250503120633.wic.xz -
Location: yocto-build/build/
deploy-ti/images/j721s2-evm/
4. Decompression
I decompressed the image using:
xz -d tisdk-edgeai-image-j721s2-evm.rootfs-20250503120633.wic.xz
Resulting in:
-
tisdk-edgeai-image-j721s2-evm.rootfs-20250503120633.wic
5. Flashing to SD Card
I flashed the image to SD card:
Used Balena Etcher to flash the .wic file
6.
Boot Partition Files After Flash
After flashing, the SD card contains:
-
tiboot3.bin -
tiboot3-j721s2-gp-evm.bin -
tiboot3-j721s2-hs-evm.bin -
tiboot3-j721s2-hs-fs-evm.bin -
tispl.bin -
u-boot.img -
uEnv.txt
These files were present in the boot partition.
Problem
After inserting the SD card into the AM68A board, the board does not boot.
what is the issue ?