Part Number: AM625
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hi Sir:
I want used the HSM in AM625.
I install the following package.
mcu_plus_sdk_am62x_11_00_00_16-linux-x64-installer.run
sysconfig-1.23.0_4000-setup.run
ti_cgt_armllvm_4.0.1.LTS_linux-x64_installer.bin
gcc-arm-9.2-2019.12-x86_64-aarch64-none-elf.tar.gz
CCS_20.1.0.00006_linux.zip -> ccs2010
Then I used the code "examples\otp\runtime_keyrev\am62x-sk\r5fss0-0_nortos\ti-arm-clang\tiboot3.bin" download to the Am625 EVM via USBDFU and got console log as following
-----------
Starting Runtime KEYREV writer
ERROR: runtime_keyrev_readKeyrevKeycnt:103: Error reading KEYREV and KEY Count !!!
Error reading KEYREV and KEY Count
Some tests have failed!!
-----------
I had check the EVM staus from UART boot
-----------

-----------
Why I can't read KEYREV and KEY value??
Thanks,
Juncor