Tool/software:
Hi,
eth0 and eth1 is not presented after modified .config of Linux. Could you help this?
[ 2.636060] am65-cpsw-nuss 8000000.ethernet: initializing am65 cpsw nuss version 0x6BA01103, cpsw version 0x6BA81103 Ports: 3 quirks:00000006
[ 2.636757] am65-cpsw-nuss 8000000.ethernet: Use random MAC address
[ 2.636779] am65-cpsw-nuss 8000000.ethernet: initialized cpsw ale version 1.5
[ 2.636786] am65-cpsw-nuss 8000000.ethernet: ALE Table size 512
[ 2.639196] remoteproc remoteproc1: remote processor 78000000.r5f is now attached
[ 2.679638] pps pps0: new PPS source ptp0
[ 2.707518] am65-cpsw-nuss 8000000.ethernet: CPTS ver 0x4e8a010c, freq:500000000, add_val:1 pps:1
[ 2.793782] remoteproc remoteproc2: 30074000.pru is available
[ 2.802814] remoteproc remoteproc3: 30078000.pru is available
[ 2.836004] cc33xx_sdio mmc2:0001:2: Using GPIO as IRQ
[ 2.879120] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[ 2.909708] Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[ 2.916081] Loaded X.509 cert 'wens: 61c038651aabdcf94bd0ac7ff06c7248db18c600'
[ 3.037608] cc33xx_driver cc33xx.4.auto: Direct firmware load for ti-connectivity/cc33xx-nvs.bin failed with error -2
done
Starting system message bus: done
Starting bluetoothd: OK
Starting network: [ 3.208973] Bluetooth: Core ver 2.22
[ 3.212711] NET: Registered PF_BLUETOOTH protocol family
[ 3.218059] Bluetooth: HCI device and connection manager initialized
ip: SIOCGIFFLAGS: No such device[ 3.224448] Bluetooth: HCI socket layer initialized
[ 3.232133] Bluetooth: L2CAP socket layer initialized
ip: SIOCGIFFLAGS: No such device
FAIL
Starting dropbear sshd: [ 3.328362] NET: Registered PF_INET6 protocol family
[ 3.334365] Segment Routing with IPv6
[ 3.338223] In-situ OAM (IOAM) with IPv6
# ifconfig eth0
ifconfig: eth0: error fetching interface information: Device not found
# ifconfig eth0 up
ifconfig: SIOCGIFFLAGS: No such device