Other Parts Discussed in Thread: DRA821
Tool/software:
I am using a DRA821U and have some concern about a NOTE that is in the datasheet.
On page 3 of the DRA821 Datasheet there is a bottom note that reads:
"B. SGMII, USB3.0, and PCIE share total of four SerDes lanes. A maximum of two of the three IP (for example, SGMII and USB) can be used concurrently."
I want to use all 4 SerDes lanes concurrently as below, is this possible?
Lane 0: PCIe Lane 0
Lane 1: SGMII Lane 4
Lane 2: SGMII Lane 1
Lane 3: USB 3.0
Thanks,
Steve