Part Number: PROCESSOR-SDK-AM335X
Tool/software:
Hello,
Hello TI Support,
We are using TISDK 09_01_00_001 in our project, which includes Linux kernel version 6.1.46. During a recent security audit, we received an extensive report highlighting many vulnerabilities in the kernel version used in the SDK. Unfortunately, we cannot upgrade the kernel easily, as doing so may introduce compatibility issues with other components provided in TISDK 09_01_00_001 (userspace libraries, drivers, etc.).
We have the following questions and would appreciate your guidance:
-
How does TI handle known CVEs in the kernel version bundled with TISDK 09_01_00_001?
-
Are security patches backported into the 6.1.46 kernel branch within the SDK, even if the version string doesn't change?
-
Is there an official security update policy for TISDK releases?
-
If we do attempt a kernel upgrade (e.g., to a newer LTS 6.1.x or 6.6), what should we watch out for regarding compatibility with TISDK 9.1 userland libraries and tools?
We want to ensure our system is secure while staying within the supported boundaries of the TISDK.
Thank you,
Neha Gupta