Part Number: IND-COMMS-SDK
Tool/software:
Hi All,
I'm trying to implement the BF and SF LEDs for our Profinet device and was wondering if the setLed stack callback can be used for this? Is there any additional info on which LED is written under what circumstances by this callback function?
The Doxygen docu of the function does not provide a lot of information and the behavior that I was seeing does not match my expectation (e.g. PN_API_IOD_LedError is active if no Ethernet Link exists on Port1 or Port2, and inactive is when an Ethernet Link is established on any port, independent of any existing AR or Profinet Communication)
Thank you and kind regards
Philip Kees