This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Reading a file from USB Storage device and keyboard on uboot in OMAP3/dm3730 (beagle board)



Hi

   I am tring to use keyboard and storge device on u-boot (beagle board).

I have added/enabled below configuration in "include/configs/omap3_beagle.h"

*==============================*/
/* USB  configuration           */
/*==============================*/

#define CONFIG_USB_KEYBOARD             1
#define CONFIG_MUSB_HCD                 1
#define CONFIG_MUSB_UDD                 1

#ifdef CONFIG_MUSB_HCD                          /* include support for usb host */
#define CONFIG_CMD_USB          1               /* include support for usb cmd */

#define CONFIG_USB_STORAGE      1               /* MSC class support */
#define CONFIG_CMD_STORAGE      1               /* inclue support for usb-storage cmd */
#define CONFIG_CMD_FAT          1               /* inclue support for FAT/storage */
#define CONFIG_DOS_PARTITION    1               /* inclue support for FAT/storage */

#ifdef CONFIG_USB_KEYBOARD                      /* HID class support */
#define CONFIG_SYS_USB_EVENT_POLL       1
#define CONFIG_PREBOOT "usb start"
#endif /* CONFIG_USB_KEYBOARD */

#endif /* CONFIG_MUSB_HCD */

   I have connected the device to USB Host but unable to detect.

OMAP3# usb�start
(Re)start USB...
USB: scanning bus for devices... No USB Device found
scanning bus for storage devices... 0 Storage Device(s) found


  Any one has tried this on beagle board.. Is it correct way / Approach ?

--
Thanks & Regards

Atul  Kumar