Hi Support Team,
In idle state, DCAN0/1_TX should be high level normally.But the DCAN0/1_TX is low level when ifconfig can0 down.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi ,
I am not seeing the waveform. Please attach.
Best Regards,
Schuyler
Hi Schuyler,
I don't know why I can't upload the attachment.
The waveform like as bellow.when uboot and device is down, the io state looks like input.
------kernel boot 3.3V--------------- -----ifconfig can0 up -----------------
| | |
---uboot-~0.3V----- ------ifconfig can0 down-----
Best Regards