This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDS64EVM: Can not import device tree file

Part Number: TMDS64EVM

Tool/software:

Hello,

I am using Buildroot for everything, my rootfs is minimal, using BusyBox init, using original TI Kernel 6.12.17 with RT configuration.

With this Kernel configuration: opened support for I2C display (solomon,ssd1306) and overlayfs, device tree works fine.

When add initramfs to kernel config, device tree not working, boot sequence switches to EFI-GRUB.

How can i fix it ?

Note: I cant use Yocto because its learning curve very bad and TI-Yocto has so much thing that i do not need even with smallest config.