Tool/software:
Hello,
I am using SDK RTOS 10.01.00.04 and attempting to perform an ENET loopback test for USXGMII (10 Gbps).
After loading the loopback firmware, I observe the following:
==========================
Enet Loopback App
==========================
=============================
Iteration 1
=============================
No valid MAC address found in EEPROM, falling back to static address
CPSW_9G Test on MAIN NAVSS
EnetBoard_setupPorts: 1 of 1 ports configurations found
Configuring SerDes lane 3 for USXGMII (10Gbps)
CpswMacPort_enableLoopback: MAC 2: Loopback is not supported in MII mode 2-2: -13
CpswMacPort_open: MAC 2: failed to set loopback mode: -13
EnetMod_open: cpsw9g.macport2: Failed to open: -13
Cpsw_openPortLinkNoPhy: Port 2: Failed to open MAC: -13
Cpsw_handleLinkDown: Port 2: Link down
EnetMod_ioctl: cpsw9g.macport2: Module is not open: -3
Cpsw_handleLinkDown: Port 2: Failed to disable MAC port: -3
Cpsw_ioctlInternal: Port 2: Failed to open port link: -13
Failed to open port link: -13
Failed to open Enet driver: -13
EnetQueue_getQCount: Queue is not initialized: -1
Assertion @ Line: 212 in src/core/enet_queue.c: queue->magic == ENET_Q_INIT_DONE
Could you please assist us in getting this test to work?
Thank you in advance for your support.
Best regards,