Hello all, hello dear PSP team
I'm are trying to integrate a third party pcie ip (lancero, www.logicandmore.com/Lancero.html)
to connect an arria2-gx FPGA to the dm8148 using pci express Gen1/x1.
I tried the same endpoint device and the same driver with EZSDK 5.03 on 2 different boards,
DM8168 EVK (DIMM3) and DM8148 EVK. The main difference is that the test on the DM8168 board
runs (still with limitations) but with the DM8148 board we get always a complete board freeze
immediately after we started the test applicaltion (pure loading of the driver works in both
cases). I'm using MSI interrupts.
Are there any undocumented differences between the pcie root complexes for the EZSDK 5_03_00_09
in case of DM8168 and DM 8148 or are there any known issues on the DM8148 EVK ??? We suspect
some interrupt issue but board freezes are really hard to debug ...
Any comments
Greetings
Christian