Tool/software:
Hi,
We're looking to use the AM6234 in a low-power person worn device. We want to use LPDDR4 to keep the power down, but I'm finding conflicting information on the amount of LPDDR4 memory that can be supported...
SPRSP58B -> Data sheet claims a maximum addressable range of up to 4GB with LPDDR4.
SPRAD06C -> Point 3.2, lists Max Addressable Range of 2GB and it seems most of the available development boards with similar processors also only come with 2GB of LPDDR4.
This forum thread seems to suggest there may be kernel patches to allow an AM623x device to access the full 4GB of 1 x 16bit Wide LPDDR4 Memory IC attached: https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1235702/am623-memory-can-t-be-configured-to-4gb-from-device-tree/4681818#4681818
(Did search the rest of the forum and found no other useful info).
Please can someone confirm the following:
a) What is the maximum supported amount of LPDDR4 that we could use with the AM6234?
b) Is the 2GB limit specifiied in SPRAD06C, limited by a software issue which could be patched out as per the above forum post, or is it hard silicon die limit?
c) If it is a software limit, would it feasible to fit a 4GB LPDDR4 Memory IC and then start with 2GB of useable space and then 'patch' it for the full 4GB in the near future?
P.S.: I'm the hardware/PCB designer.
Regards,
Nick