Tool/software:
Hi,
The PDN for the AM62L is mentioning that the VDDA_3P3_USB and VDDA_3P3_SDIO power rails should be powered via an external DCDC in paralell to the TPS6521401. But can this DCDC be removed if the PMIC is powered with 3.3V only? So that VDDA_3P3_USB, VDDA_3P3_SDIO (with the power switch) and the TPS6521401 are connected to the same 3.3V power rail or does this create issues on the power sequencing?
Thank you!
Marinus