Tool/software:
Hi TI Experts
I see the below status on TI.com for AM62L

Can you provide additional inputs on the collaterals to be referred or guidelines to follow during custom board design
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi TI Experts
I see the below status on TI.com for AM62L

Can you provide additional inputs on the collaterals to be referred or guidelines to follow during custom board design
Hi Board Designers,
Refer below:
FAQs
Core
Peripherals
EVM
Design
Other E2Es for reference:
Bootmode
This is a known issue, errata is in the process of being updated. Your observations align with ours, in that several different types of SanDisk cards fail, while cards from other manufacturers boot successfully. For silicon revision 1.0, there is not a robust workaround, other than to continue using the working cards. We have also seen that if you set both primary and backup to SD card boot, sometimes the backup boot will be successful on certain card that failed the primary boot
As per the Errata i2473 Boot: eMMC boot may fail, outlined in the “AM62Lx Sitara Processors Silicon Errata, Silicon Revision 1.0” document, the recommended workaround is to utilize eMMC boot via UDA.
In our SOM design, we support only the reduced pin count boot mode, where eMMC boot is limited to the MMC0 (eMMC) Boot Partition. While we have provisions for booting from a microSD card—which we are currently utilizing—eMMC boot support is mandatory for us. Currently, we do not have an option to enable eMMC boot using UDA.
We would like to confirm whether this erratum will be addressed in the next silicon revision and if Yes, the issue is fully root caused, and the fix is being implemented for next silicon revision.
Yes, the eMMC boot from boot partition (once the issue is fixed) is supported via reduced boot pin configurations.
DDR4
eMMC
SD card
https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1502807/am62l-spi-voltages
The FAQ is being updated.
Please review the FAQ frequently for updates.
Regards,
Sreenivasa
Hi Board Designers,
Refer below additional information:
DDR4 memory addressable range
The device was targeted for lower cost industrial applications; thus package was optimized, and some DDR pins were sacrificed, including one of the CS pins. This only allows single rank designs (AM62x has 2CS for dual rank designs), which halved the maximum address reach for DDR.
Note LPDDR4 max is 2GByte, but DDR4 max is 4GByte
The DDRSS does not support DDR0_ALERT_n, DDR0_PAR, DDR0_CKE1, DDR0_CS1_n, DDR0_ODT1 signals (pins). It is recommended to follow the memory data sheet recommendations to connect any of the available signals that are not interfaced to the processor DDRSS
AM62L - SOC Package Delays for DDR interface
Refer AM62x, AM62Lx DDR Board Design and Layout Guidelines.
AM62L31, can the integrated switch be run in totally unmanaged mode if e.g. the 62L31 CPU boot fails and is not able to do any configuration to the switch?
Minimum requirement would be the capability to forward the traffic between the external RGMII ports.
No. At boot the Ethernet ports are configured as just ports, not as a switch. Further the subsystem is not reset-isolated in hardware, so there is no guarantee that in all cases the switch keeps operating regardless of what happens on the A53's. So there will be an interruption of the switching function for the duration of the SoC reset and operating system boot.
GPMC interface modes supported
Supported GPMC configuration includes 16-bit (GPMC, Raw NAND, Muxed-NOR). The GPMC signal names are representative of the IP functionality rather than the supported functionality. Non-multiplexed Address and Data interface mode is not supported.
Does the AM62L support the redundant copies of the first stage boot loader at UDA for eMMC?
Please refer to the section “5.4.3.1 eMMC Bootloader Operation” of the TRM. It mentions that the ROM supports booting the redundant image at offset 0x400000 incase the booting fails from the primary offset 0x0 for the UDA RAW mode only.
For the UDA FS mode, the ROM doesn’t have the redundant boot support.
If you are booting Linux then you may not use the UDA RAW mode as the primary offset 0x0 conflicts with the partition table required for the filesystems.
So, the feasible option is to use UDA FS mode for which the ROM doesn’t have redundant boot support.
Regards,
Sreenivasa
I also see a corresponding User Guide: Hardware Design Considerations for Custom Board Using AM62L32 and AM62L01 Processors available under AM62L-PROCESSOR-SDK Software development kit (SDK) | TI.com. Adding in case this isn't covered by the above content and if it serves as a good reference for the related matter.
Thanks,
Harshit
Hello Harshit,
Thank you for the inputs and this help. Appreciate your input for improving the collateral.
FYI, we have the above referenced file and other key collateral links included in the below FAQ
Regards,
Sreenivasa
Hi Board Designers,
Refer below inputs regarding eMMC support for SR1.1
AM62L: eMMC boot failure in reduced pin mode
As noted from <Table 5-3. BOOTMODE Pin Mapping (Reduced)> in AM62L TRM https://www.ti.com/lit/pdf/sprujb4
BOOTMODE[15:12] = 1011 => Fixed 4 => eMMC Boot Partition (primary) MMC (backup)
BOOTMODE[15:12] = 1010 => Fixed 3 => MMC/UDA (primary) UART (backup)
BOOTMODE[15:12] = 1000 => Fixed 1 => eMMC Boot Partition (primary) USB-DFU (backup)
As noted from <Table 1-2. Advisories Matrix> in AM62L Errata https://www.ti.com/lit/pdf/sprz582, there're eMMC boot issues from eMMC boot partition in AM62L PG1.0 ROM, and your test struck the eMMC boot issues.
With AM62L PG1.1 fixes on ROM as noted in <Table 1-2. Advisories Matrix> in AM62L Errata https://www.ti.com/lit/pdf/sprz582, I'd recommend re-run your test on AM62L PG1.1 silicon.
In reference to <Table 9-1. Nomenclature Description> in AM62L datasheet https://www.ti.com/lit/ds/symlink/am62l.pdf, The <Device revision> field increments from "A" to "B" for SR 1.1 silicon.

Please work with TI local team on how to order AM62L SR 1.1 silicon.
Regards,
Sreenivasa
(+) AM62L: MMC - Processors forum - Processors - TI E2E support forums
Do all three MMC/SD buses support eMMC 5.1, SD 3.0, and SDIO Version 3.0?
2、What does the content shown in the following picture mentioned in the TRM manual mean? Does it support SD 4.10 and SDIO 4.0? So, should we follow the data manual or the TRM?


The next revision of the AM62Lx datasheet will be updated to show with the following list of devices and data transfer modes supported for each MMC instance.
The MMC0 port supports connections to an eMMC device or embedded SDIO device. It does not support removable SD Cards.
The MMC1 and MMC2 ports support connection to a removable SD Cards or embedded SDIO device. They do not support eMMC devices.


Regards,
Sreenivasa