Other Parts Discussed in Thread: PCM3168A
Tool/software:
As codec the pcm3168a is used and connected with DOUT1/2 ports.
Codec configuration:
Format: Left-Justified Mode
Sampling-Rate: 96 kHz
SCKI Rate: 256
The mcasp is configured in 4 Slot TDM mode over two rx serializers.
I would expect to receive all 6 ADC channels from the codec.
However, I'm only able to receive four channels over the first serializer.
$ arecord -f s24_3le -r 96000 -c 6 -D hw:0,0 a.wav arecord: set_params:1398: Channels count non available
The used device tree:
simple-audio-card,dai-link {
format = "left_j";
mclk-fs = <256>;
cpu {
bitclock-master;
frame-master;
dai-tdm-slot-num = <6>;
dai-tdm-slot-width = <32>;
dai-tdm-slot-tx-mask = <0 0 0 0 0 0>;
dai-tdm-slot-rx-mask = <1 1 1 1 1 1>;
sound-dai = <&mcasp1>;
};
codec {
clocks = <&audio_refclk0>;
sound-dai = <&pcm3168a 1>;
};
};
&mcasp1 {
pinctrl-names = "default";
pinctrl-0 = <&mcasp1_pins>;
op-mode = <0>;
serial-dir = < /* 0: INACTIVE, 1: TX, 2: RX */
2 2 0 0
0 0 0 0
0 0 0 0
0 0 0 0
>;
tdm-slots = <4>;
#sound-dai-cells = <0>;
/*
* assign mcasp0 clocks because pcm3168a uses audio_refclk0
*/
clocks = <&k3_clks 190 0>;
clock-names = "fck";
assigned-clocks = <&k3_clks 190 0>;
assigned-clock-parents = <&k3_clks 190 2>;
assigned-clock-rates = <24576000>;
status = "okay";
};After some digging in the `davinci-mcasp.c` driver I found that I had to set the rx/tx masks but this made the driver complain about mismatched tdm_slot size and mask size.
davinci-mcasp 2b10000.audio-controller: Bad tdm mask tx: 0x00000000 rx: 0x0000003f slots 4
I saw that the `dai-tdm-slot-num` property will overwrite the mcasp `tdm-slots` property. This seems to make it impossible to configure the drive the way I want, so I removed the overwrite.
I read the `dai-tdm-slot-num` property as the total number of required tdm-slots and `tdm-slots` property as the tdm-slots per serializer.
davinci-mcasp.c - mcasp->tdm_slots = slots; + // mcasp->tdm_slots = slots;
With this patch applied, I was able to record audio from the 6th channel, but the samples were scattered over 3 channels.
This was recorded with a signal generator connected to ADC channel six on the codec.