Part Number: AM68
Other Parts Discussed in Thread: AM62P,
Tool/software:
Hi,Experts
In the AM68x series datasheet,“up to xxxMP/s”is listed under Features as
a Video Encoder/Decoder performance value.
The “xxx” value varies for each series.
Is the performance required to encode 4K (3840 x 2160) resolution correct?
For 30fps
3840 * 2160 * 30 = approx. 249 MP/s
For 60fps
3840 * 2160 * 60 = approx. 498 MP/s
In the case of AM62P, it says “up to 300MP/s” in the Features section,
so I am wondering if the performance is up to 4K and 30fps,
However, in chapters 1.4.32 and 7.4 of the Technical Reference Manual (SPRUJ83A),
“60fps” is also mentioned.
Best Regards,
Hidekazu