Tool/software:
Hello, TI Expert,
In PSDK 10.1 the file
c7x-mma-tidl/arm-tidl/config.mk
defines build variables only for QNX SDP 7.0 and 7.1.
To work with QNX SDP 8.0 (800) I inserted the section below.
Could you please confirm whether this is the correct approach and advise on any additional changes needed?
export QNX_SDP_VERSION ?= 710 ifeq ($(QNX_SDP_VERSION),700) export QNX_BASE ?= $(HOME)/qnx700 export QNX_CROSS_COMPILER_TOOL ?= aarch64-unknown-nto-qnx7.0.0- else ifeq ($(QNX_SDP_VERSION),800) export QNX_BASE ?= $(HOME)/qnx800 export QNX_CROSS_COMPILER_TOOL ?= aarch64-unknown-nto-qnx8.0.0- export QNX_TARGET ?= $(QNX_BASE)/target/qnx PATH := $(QNX_BASE)/host/linux/x86_64/usr/bin:$(PATH) else export QNX_BASE ?= $(HOME)/qnx710 export QNX_CROSS_COMPILER_TOOL ?= aarch64-unknown-nto-qnx7.1.0- # Adding this path for QNX SDP 7.1 so g++ can invoke ld correctly PATH := $(QNX_BASE)/host/linux/x86_64/usr/bin:$(PATH) endif export QNX_HOST ?= $(QNX_BASE)/host/linux/x86_64 export QNX_TARGET ?= $(QNX_BASE)/target/qnx7 export GCC_QNX_ROOT ?= $(QNX_HOST)/usr/bin export GCC_QNX_ARM_ROOT ?= $(QNX_HOST)/usr/bin export GCC_QNX_ARM ?= $(QNX_HOST)/usr/bin
Question
1. Besides the changes above, are there any other files or variables that must be updated to build TDA4x (C7x-MMA TIDL) with QNX SDP 8.0 on PSDK 10.1?
-
e.g., adjustments to
QNX_TARGET/QNX_HOST, build scripts, GCC version requirements, etc.
Best Regards,
Hyeonseong.