Tool/software:
Hello TI partner,
CODEBASE INFO
【SDK】J721S2 10.01.00.04
【PDK】pdk_j721s2_10_01_00_25
20250513-1-TI_Question.zip
【CODE】/codes
【PATCH】057a657.diff
【CAN TOOL】TSMaster. 20250513-1-Code_and_TSMaster_Config.docx
【ASC FILE】XCP_Trigger_svnv27639_V2.ASC
Our requirement is use Classic CAN for tx/rx operation but most examples in pdk_j721s2_10_01_00_25 are CAN-FD format.
We refered \pdk_j721s2_10_01_00_25\packages\ti\csl\example\mcan\mcanEvmLoopback for implementation and adjusted mcan config as patch 057a657.diff or codes dir.
For mcan tx test, TSMaster can interpret CAN msg from DUT successfully.
For mcan rx test, we used TSMaster to play CAN data but cannot capture any MCAN_RxBufElement from canBus0RxQueue. Pls refer 20250513-1-Code_and_TSMaster_Config.docx.
Because mcan tx test is ok, we think TSMaster configuration should be correct and problem should be occurred in our mcan configuration.
Could you help us check where the problem is?
Thanks!
Troy Chen
(O) +886-2-22685511#61836
(M) +886-9-10-709335
troyywchen@fih-foxconn.com