Tool/software:
Hi,
There is a way to optimize cache flush and invaliate operations?
If I produce 8MB bytes of data, written in DDR, and I want to pass them to another core, a cache flush i required. Normally I flush form data start up to data start + size (1M), but since the cache is 512M only, I would like to flush 512K only.
If the data are produced in sequence, from lower address to upper address, can I assume only the last 512K of data requires flush?