Other Parts Discussed in Thread: DRA821
Tool/software:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
root@j7200-evm:~# dmesg | grep i2c [ 0.750746] i2c_dev: i2c /dev entries driver [ 0.888688] omap_i2c 42120000.i2c: bus 0 rev0.12 at 400 kHz [ 0.952077] omap_i2c 2000000.i2c: bus 1 rev0.12 at 400 kHz [ 0.989524] omap_i2c 2010000.i2c: bus 2 rev0.12 at 400 kHz
Hi Keerthy,
PFA the log for i2C and sdk version.
SDK Version - ti-processor-sdk-linux-j7200-evm-10_00_07_03
We have another query. I am running the dmesg | grep -i dtb in the terminal, what I'd like to know is that if the file is properly loaded will it show the dtb file name that we have uploaded in u-boot.
The is the process -
1. We made changes to the device tree file and we have compiled to to dtb.
2. After that we copied the generated dtb file to the boot directory of the sd card in which we have flashed the .wic image via yocto.
3. Then we used the following commands in u-boot -
ls mmc 1:1
setenv fdtfile k3-j7200-common-proc-board.dtb (in copied SD card)
run bootcmd_mmc1
Regards,
Jai Raghav
Hi Jai,
It seems like 42120000 i2c instance is getting probed fine as per dmesg. Can you double check the pinmux?
Also to which slave id is the device connected?
Also 42120000 is not main domain i2c.
. After that we copied the generated dtb file to the boot directory of the sd card in which we have flashed the .wic image via yocto.
Typically the dtb is picked up from the rootfs boot folder.
Best Regards,
Keerthy
Hi Jai,
Where is the Linux kernel image loaded from? It is typically loaded from the boot folder under rootfs.
I still have not got the complete Linux boot logs. Can you please share?
- Keerthy
Thankyou keerthi for immediate reply ,SD card has both boot and rootf
Complete linux Boot logs root@j7200-evm:/# reboot Stopping Session c2 of User root... [ OK ] Removed slice Slice /system/modprobe. [ OK ] Stopped target Graphical Interface. [ OK ] Stopped target Multi-User System. [ OK ] Stopped target Login Prompts. [ OK ] Stopped target RPC Port Mapper. [ OK ] Stopped target Timer Units. [ OK ] Stopped Daily rotation of log files. [ OK ] Stopped Daily Cleanup of Temporary Directories. [ OK ] Stopped target System Time Set. [ OK ] Closed Process Core Dump Socket. [ OK ] Closed Load/Save RF Kill Switch Status /dev/rfkill Watch. Stopping Job spooling tools... Stopping Avahi mDNS/DNS-SD Stack... Stopping containerd container runtime... Stopping Periodic Command Scheduler... [ OK ] Stopped DEMO. Stopping Getty on tty1... Stopping irqbalance daemon... Stopping Reboot and dump vmcore via kexec... Stopping Netperf Benchmark Server... Stopping NFS status monitor for NFSv2/3 locking.... Stopping Telephony service... [ OK ] Stopped Expand the rootfs …full size of the boot device.. Stopping Serial Getty on ttyS2... Stopping Simple Network Ma…ent Protocol (SNMP) Daemon.... Stopping Simple Network Ma…rotocol (SNMP) Trap Daemon.... Stopping strongSwan IPsec …Ev2 daemon using ipsec.conf... Stopping Load/Save Random Seed... Stopping TEE Supplicant... Stopping Telnet Server... [ OK ] Stopped Job spooling tools. [ OK ] Stopped Periodic Command Scheduler. [ OK ] Stopped irqbalance daemon. [ OK ] Stopped Telephony service. [ OK ] Stopped strongSwan IPsec I…IKEv2 daemon using ipsec.conf. [ OK ] Stopped TEE Supplicant. [ OK ] Stopped Avahi mDNS/DNS-SD Stack. [ OK ] Stopped Netperf Benchmark Server. [ OK ] Stopped NFS status monitor for NFSv2/3 locking.. [ OK ] Stopped Simple Network Man…ement Protocol (SNMP) Daemon.. [ OK ] Stopped Simple Network Man… Protocol (SNMP) Trap Daemon.. [ OK ] Stopped containerd container runtime. [ OK ] Stopped Getty on tty1. [ OK ] Stopped Serial Getty on ttyS2. [ OK ] Stopped Reboot and dump vmcore via kexec. [ OK ] Stopped Load/Save Random Seed. [ OK ] Stopped Telnet Server. [ OK ] Stopped Session c2 of User root. [ OK ] Removed slice Slice /system/getty. [ OK ] Removed slice Slice /system/serial-getty. [ OK ] Stopped target Host and Network Name Lookups. Stopping User Login Management... Stopping User Manager for UID 0... [ OK ] Stopped User Manager for UID 0. Stopping User Runtime Directory /run/user/0... [ OK ] Unmounted /run/user/0. [ OK ] Stopped User Login Management. [ OK ] Stopped User Runtime Directory /run/user/0. [ OK ] Removed slice User Slice of UID 0. Stopping Permit User Sessions... [ OK ] Stopped Permit User Sessions. [ OK ] Stopped target Network. [ OK ] Stopped target Remote File Systems. Stopping Network Name Resolution... [ OK ] Stopped Network Name Resolution. Stopping Network Configuration... [ OK ] Stopped Network Configuration. [ OK ] Stopped target Preparation for Network. [ OK ] Stopped IPv6 Packet Filtering Framework. [ OK ] Stopped IPv4 Packet Filtering Framework. [ OK ] Stopped target Basic System. [ OK ] Stopped target Path Units. [ OK ] Stopped Dispatch Password …ts to Console Directory Watch. [ OK ] Stopped Forward Password R…uests to Wall Directory Watch. [ OK ] Stopped target Slice Units. [ OK ] Removed slice User and Session Slice. [ OK ] Stopped target Socket Units. [ OK ] Closed Avahi mDNS/DNS-SD Stack Activation Socket. [ OK ] Closed Docker Socket for the API. [ OK ] Closed dropbear.socket. [ OK ] Closed PC/SC Smart Card Daemon Activation Socket. [ OK ] Closed Network Service Netlink Socket. [ OK ] Closed Weston socket. Stopping D-Bus System Message Bus... [ OK ] Stopped D-Bus System Message Bus. [ OK ] Closed D-Bus System Message Bus Socket. [ OK ] Stopped target System Initialization. [ OK ] Stopped Apply Kernel Variables. [ OK ] Stopped Load Kernel Modules. Stopping Network Time Synchronization... Stopping Record System Boot/Shutdown in UTMP... [ OK ] Stopped Network Time Synchronization. [ OK ] Stopped Record System Boot/Shutdown in UTMP. [ OK ] Stopped Create Volatile Files and Directories. [ OK ] Stopped target Local File Systems. Unmounting /media/ram... Unmounting /run/media/boot-mmcblk1p1... Unmounting Temporary Directory /tmp... Unmounting /var/volatile... [ OK ] Unmounted /media/ram. [ OK ] Unmounted /run/media/boot-mmcblk1p1. [ OK ] Unmounted Temporary Directory /tmp. [ OK ] Unmounted /var/volatile. [ OK ] Stopped target Swaps. [ OK ] Reached target Unmount All Filesystems. [ OK ] Stopped File System Check on /dev/mmcblk1p1. [ OK ] Removed slice Slice /system/systemd-fsck. [ OK ] Stopped target Preparation for Local File Systems. [ OK ] Stopped Remount Root and Kernel File Systems. [ OK ] Stopped Create Static Device Nodes in /dev. [ OK ] Reached target System Shutdown. [ OK ] Reached target Late Shutdown Services. [ OK ] Finished System Reboot. [ OK ] Reached target System Reboot. [ 1062.005146] kauditd_printk_skb: 1 callbacks suppressed [ 1062.005159] audit: type=1334 audit(1651308240.512:15): prog-id=4 op=UNLOAD [ 1062.017931] audit: type=1334 audit(1651308240.512:16): prog-id=3 op=UNLOAD [ 1062.024849] audit: type=1334 audit(1651308240.512:17): prog-id=10 op=UNLOAD [ 1062.031830] audit: type=1334 audit(1651308240.512:18): prog-id=9 op=UNLOAD [ 1062.038717] audit: type=1334 audit(1651308240.512:19): prog-id=8 op=UNLOAD [ 1062.045588] audit: type=1334 audit(1651308240.512:20): prog-id=7 op=UNLOAD [ 1062.052459] audit: type=1334 audit(1651308240.524:21): prog-id=6 op=UNLOAD [ 1062.059326] audit: type=1334 audit(1651308240.524:22): prog-id=5 op=UNLOAD [ 1062.069353] watchdog: watchdog0: nowayout prevents watchdog being stopped! [ 1062.076572] watchdog: watchdog0: watchdog did not stop! [ 1062.093359] systemd-shutdown[1]: Using hardware watchdog 'K3 RTI Watchdog', version 0, device /dev/watchdog0 [ 1062.103223] systemd-shutdown[1]: Modifying watchdog timeout is not supported, reusing the programmed timeout. [ 1062.113164] systemd-shutdown[1]: Watchdog running with a timeout of 1min. [ 1062.130157] systemd-shutdown[1]: Syncing filesystems and block devices. [ 1062.148841] systemd-shutdown[1]: Sending SIGTERM to remaining processes... [ 1062.164419] systemd-journald[163]: Received SIGTERM from PID 1 (systemd-shutdow). [ 1062.173248] audit: type=1335 audit(1651308240.680:23): pid=163 uid=0 auid=4294967295 tty=(none) ses=4294967295 comm="systemd-journal" exe="/lib/systemd/systemd-journald" nl-mcgrp=1 op=disconnect res=1 [ 1062.196198] systemd-shutdown[1]: Sending SIGKILL to remaining processes... [ 1062.208658] systemd-shutdown[1]: Unmounting file systems. [ 1062.215943] [1400]: Remounting '/' read-only with options 'n/a'. [ 1062.239890] EXT4-fs (mmcblk1p2): re-mounted. Quota mode: none. [ 1062.251139] systemd-shutdown[1]: All filesystems unmounted. [ 1062.256752] systemd-shutdown[1]: Deactivating swaps. [ 1062.261906] systemd-shutdown[1]: All swaps deactivated. [ 1062.267164] systemd-shutdown[1]: Detaching loop devices. [ 1062.274879] systemd-shutdown[1]: All loop devices detached. [ 1062.280482] systemd-shutdown[1]: Stopping MD devices. [ 1062.285744] systemd-shutdown[1]: All MD devices stopped. [ 1062.291056] systemd-shutdown[1]: Detaching DM devices. [ 1062.296318] systemd-shutdown[1]: All DM devices detached. [ 1062.301750] systemd-shutdown[1]: All filesystems, swaps, loop devices, MD devices and DM devices detached. [ 1062.319279] systemd-shutdown[1]: Syncing filesystems and block devices. [ 1062.326222] systemd-shutdown[1]: Rebooting. [ 1062.393127] reboot: Restarting system U-Boot SPL 2023.04-ti-gf9b966c67473 (Mar 19 2024 - 20:31:40 +0000) SYSFW ABI: 3.1 (firmware rev 0x0009 '9.2.4--v09.02.04 (Kool Koala)') Trying to boot from MMC2 Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Loading Environment from nowhere... OK Starting ATF on ARM64 core... NOTICE: BL31: v2.10.0(release):v2.10.0-367-g00f1ec6b87-dirty NOTICE: BL31: Built : 16:09:05, Feb 9 2024 I/TC: I/TC: OP-TEE version: 4.1.0-51-g012cdca49 (gcc version 11.4.0 (GCC)) #1 Tue Jan 30 10:48:03 UTC 2024 aarch64 I/TC: WARNING: This OP-TEE configuration might be insecure! I/TC: WARNING: Please check https://optee.readthedocs.io/en/latest/architecture/porting_guidelines.html I/TC: Primary CPU initializing I/TC: GIC redistributor base address not provided I/TC: Assuming default GIC group status and modifier I/TC: SYSFW ABI: 3.1 (firmware rev 0x0009 '9.2.4--v09.02.04 (Kool Koala)') I/TC: HUK Initialized I/TC: Activated SA2UL device I/TC: Fixing SA2UL firewall owner for GP device I/TC: Enabled firewalls for SA2UL TRNG device I/TC: SA2UL TRNG initialized I/TC: SA2UL Drivers initialized I/TC: Primary CPU switching to normal world boot U-Boot SPL 2023.04-ti-gf9b966c67473 (Mar 19 2024 - 20:31:40 +0000) SYSFW ABI: 3.1 (firmware rev 0x0009 '9.2.4--v09.02.04 (Kool Koala)') Detected: J7X-BASE-CPB rev A Detected: J7X-VSC8514-ETH rev E2 Trying to boot from MMC2 am654_sdhci mmc@4fb0000: pinctrl_select_state_full: uclass_get_device_by_phandle_id: err=-19 Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted U-Boot 2023.04-ti-gf9b966c67473 (Mar 19 2024 - 20:31:40 +0000) SoC: J7200 SR2.0 GP Model: Texas Instruments K3 J7200 SoC Board: J7200X-PM2-SOM rev E8 DRAM: 2 GiB (effective 4 GiB) Core: 85 devices, 32 uclasses, devicetree: separate Flash: 0 Bytes MMC: mmc@4f80000: 0, mmc@4fb0000: 1 Loading Environment from nowhere... OK In: serial@2800000 Out: serial@2800000 Err: serial@2800000 am65_cpsw_nuss ethernet@46000000: K3 CPSW: nuss_ver: 0x6BA02102 cpsw_ver: 0x6BA82102 ale_ver: 0x00293904 Ports:1 mdio_freq:1000000 Detected: J7X-BASE-CPB rev A Detected: J7X-VSC8514-ETH rev E2 Net: eth0: ethernet@46000000port@1 Hit any key to stop autoboot: 0 switch to partitions #0, OK mmc1 is current device SD/MMC found on device 1 Failed to load 'boot.scr' 612 bytes read in 6 ms (99.6 KiB/s) Loaded env from uEnv.txt Importing environment from mmc1 ... gpio: pin gpio@22_17 (gpio 126) value is 1 gpio: pin gpio@22_16 (gpio 125) value is 0 k3_r5f_rproc r5f@41000000: Core 1 is already in use. No rproc commands work 73912 bytes read in 34 ms (2.1 MiB/s) Load Remote Processor 1 with data@addr=0x82000000 73912 bytes: Success! 576944 bytes read in 20 ms (27.5 MiB/s) Load Remote Processor 2 with data@addr=0x82000000 576944 bytes: Success! 73912 bytes read in 15 ms (4.7 MiB/s) Load Remote Processor 3 with data@addr=0x82000000 73912 bytes: Success! 19376640 bytes read in 207 ms (89.3 MiB/s) 69764 bytes read in 9 ms (7.4 MiB/s) Working FDT set to 88000000 ## Flattened Device Tree blob at 88000000 Booting using the fdt blob at 0x88000000 Working FDT set to 88000000 Loading Device Tree to 000000008feeb000, end 000000008fffffff ... OK Working FDT set to 8feeb000 Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x411fd080] [ 0.000000] Linux version 6.1.80-ti-g2e423244f8c0 (oe-user@oe-host) (aarch64-oe-linux-gcc (GCC) 11.4.0, GNU ld (GNU Binutils) 2.38.20220708) #1 SMP PREEMPT Wed Mar 20 14:43:33 UTC 2024 [ 0.000000] Machine model: Texas Instruments J7200 EVM [ 0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '') [ 0.000000] printk: bootconsole [ns16550a0] enabled [ 0.000000] efi: UEFI not found. [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a0000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node r5f-memory@a0100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a1000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node r5f-memory@a1100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a2000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a2000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a2100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node r5f-memory@a2100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a3000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a3000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a3100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node r5f-memory@a3100000, compatible id shared-dma-pool [ 0.000000] Zone ranges: [ 0.000000] DMA [mem 0x0000000080000000-0x00000000ffffffff] [ 0.000000] DMA32 empty [ 0.000000] Normal [mem 0x0000000100000000-0x00000008ffffffff] [ 0.000000] Movable zone start for each node [ 0.000000] Early memory node ranges [ 0.000000] node 0: [mem 0x0000000080000000-0x000000009e7fffff] [ 0.000000] node 0: [mem 0x000000009e800000-0x00000000a47fffff] [ 0.000000] node 0: [mem 0x00000000a4800000-0x00000000ffffffff] [ 0.000000] node 0: [mem 0x0000000880000000-0x00000008ffffffff] [ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000008ffffffff] [ 0.000000] cma: Reserved 32 MiB at 0x00000000fe000000 [ 0.000000] psci: probing for conduit method from DT. [ 0.000000] psci: PSCIv1.1 detected in firmware. [ 0.000000] psci: Using standard PSCI v0.2 function IDs [ 0.000000] psci: Trusted OS migration not required [ 0.000000] psci: SMC Calling Convention v1.4 [ 0.000000] percpu: Embedded 20 pages/cpu s41064 r8192 d32664 u81920 [ 0.000000] Detected PIPT I-cache on CPU0 [ 0.000000] CPU features: detected: GIC system register CPU interface [ 0.000000] CPU features: detected: Spectre-v3a [ 0.000000] CPU features: detected: Spectre-BHB [ 0.000000] CPU features: detected: ARM erratum 1742098 [ 0.000000] CPU features: detected: ARM errata 1165522, 1319367, or 1530923 [ 0.000000] alternatives: applying boot alternatives [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 1032192 [ 0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 root=PARTUUID=164f123c-02 rw rootfstype=ext4 rootwait [ 0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes, linear) [ 0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes, linear) [ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off [ 0.000000] software IO TLB: area num 2. [ 0.000000] software IO TLB: mapped [mem 0x00000000fa000000-0x00000000fe000000] (64MB) [ 0.000000] Memory: 3897284K/4194304K available (11712K kernel code, 1258K rwdata, 3812K rodata, 1984K init, 438K bss, 264252K reserved, 32768K cma-reserved) [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1 [ 0.000000] rcu: Preemptible hierarchical RCU implementation. [ 0.000000] rcu: RCU event tracing is enabled. [ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=2. [ 0.000000] Trampoline variant of Tasks RCU enabled. [ 0.000000] Tracing variant of Tasks RCU enabled. [ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies. [ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2 [ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0 [ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode [ 0.000000] GICv3: 960 SPIs implemented [ 0.000000] GICv3: 0 Extended SPIs implemented [ 0.000000] Root IRQ handler: gic_handle_irq [ 0.000000] GICv3: GICv3 features: 16 PPIs [ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001900000 [ 0.000000] ITS [mem 0x01820000-0x0182ffff] [ 0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS [ 0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19 [ 0.000000] ITS@0x0000000001820000: allocated 524288 Devices @880800000 (flat, esz 8, psz 64K, shr 0) [ 0.000000] ITS: using cache flushing for cmd queue [ 0.000000] GICv3: using LPI property table @0x0000000880030000 [ 0.000000] GIC: using cache flushing for LPI property table [ 0.000000] GICv3: CPU0: using allocated LPI pending table @0x0000000880040000 [ 0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention. [ 0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys). [ 0.000000] clocksource: arch_sys_counter: mask: 0x3ffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns [ 0.000000] sched_clock: 58 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns [ 0.008339] Console: colour dummy device 80x25 [ 0.012907] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000) [ 0.023579] pid_max: default: 32768 minimum: 301 [ 0.028315] LSM: Security Framework initializing [ 0.033090] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes, linear) [ 0.040666] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes, linear) [ 0.049478] cblist_init_generic: Setting adjustable number of callback queues. [ 0.056881] cblist_init_generic: Setting shift to 1 and lim to 1. [ 0.063147] cblist_init_generic: Setting adjustable number of callback queues. [ 0.070534] cblist_init_generic: Setting shift to 1 and lim to 1. [ 0.076855] rcu: Hierarchical SRCU implementation. [ 0.081753] rcu: Max phase no-delay instances is 1000. [ 0.087265] Platform MSI: msi-controller@1820000 domain created [ 0.093420] PCI/MSI: /bus@100000/interrupt-controller@1800000/msi-controller@1820000 domain created [ 0.102768] EFI services will not be available. [ 0.107505] smp: Bringing up secondary CPUs ... I/TC: Secondary CPU 1 initializing I/TC: Secondary CPU 1 switching to normal world boot [ 0.120687] Detected PIPT I-cache on CPU1 [ 0.120748] GICv3: CPU1: found redistributor 1 region 0:0x0000000001920000 [ 0.120764] GICv3: CPU1: using allocated LPI pending table @0x0000000880050000 [ 0.120796] CPU1: Booted secondary processor 0x0000000001 [0x411fd080] [ 0.120845] smp: Brought up 1 node, 2 CPUs [ 0.150193] SMP: Total of 2 processors activated. [ 0.154997] CPU features: detected: 32-bit EL0 Support [ 0.160251] CPU features: detected: CRC32 instructions [ 0.165529] CPU: All CPU(s) started at EL2 [ 0.169711] alternatives: applying system-wide alternatives [ 0.176239] devtmpfs: initialized [ 0.184278] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns [ 0.194257] futex hash table entries: 512 (order: 3, 32768 bytes, linear) [ 0.201853] pinctrl core: initialized pinctrl subsystem [ 0.207517] DMI not present or invalid. [ 0.211760] NET: Registered PF_NETLINK/PF_ROUTE protocol family [ 0.218342] DMA: preallocated 512 KiB GFP_KERNEL pool for atomic allocations [ 0.225657] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations [ 0.233694] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations [ 0.241818] audit: initializing netlink subsys (disabled) [ 0.247414] audit: type=2000 audit(0.160:1): state=initialized audit_enabled=0 res=1 [ 0.247612] thermal_sys: Registered thermal governor 'step_wise' [ 0.255336] thermal_sys: Registered thermal governor 'power_allocator' [ 0.261493] cpuidle: using governor menu [ 0.272230] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers. [ 0.279194] ASID allocator initialised with 65536 entries [ 0.290734] platform a40000.pinctrl: Fixed dependency cycle(s) with /bus@100000/pinctrl@a40000/mcu-cpsw-cpts [ 0.301637] KASLR disabled due to lack of seed [ 0.309066] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages [ 0.316031] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page [ 0.322439] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages [ 0.329384] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page [ 0.335811] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages [ 0.342745] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page [ 0.349147] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages [ 0.356080] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page [ 0.363265] k3-chipinfo 43000014.chipid: Family:J7200 rev:SR2.0 JTAGID[0x1bb6d02f] Detected [ 0.372507] iommu: Default domain type: Translated [ 0.377497] iommu: DMA domain TLB invalidation policy: strict mode [ 0.384020] SCSI subsystem initialized [ 0.388022] usbcore: registered new interface driver usbfs [ 0.393644] usbcore: registered new interface driver hub [ 0.399083] usbcore: registered new device driver usb [ 0.404422] pps_core: LinuxPPS API ver. 1 registered [ 0.409495] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it> [ 0.418839] PTP clock support registered [ 0.422906] EDAC MC: Ver: 3.0.0 [ 0.426565] FPGA manager framework [ 0.430079] Advanced Linux Sound Architecture Driver Initialized. [ 0.436721] clocksource: Switched to clocksource arch_sys_counter [ 0.443091] VFS: Disk quotas dquot_6.6.0 [ 0.447124] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes) [ 0.457124] NET: Registered PF_INET protocol family [ 0.462507] IP idents hash table entries: 65536 (order: 7, 524288 bytes, linear) [ 0.471657] tcp_listen_portaddr_hash hash table entries: 2048 (order: 3, 32768 bytes, linear) [ 0.480413] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear) [ 0.488340] TCP established hash table entries: 32768 (order: 6, 262144 bytes, linear) [ 0.496569] TCP bind hash table entries: 32768 (order: 8, 1048576 bytes, linear) [ 0.505325] TCP: Hash tables configured (established 32768 bind 32768) [ 0.512170] UDP hash table entries: 2048 (order: 4, 65536 bytes, linear) [ 0.519090] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes, linear) [ 0.526540] NET: Registered PF_UNIX/PF_LOCAL protocol family [ 0.532624] RPC: Registered named UNIX socket transport module. [ 0.538685] RPC: Registered udp transport module. [ 0.543488] RPC: Registered tcp transport module. [ 0.548293] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.554876] NET: Registered PF_XDP protocol family [ 0.559777] PCI: CLS 0 bytes, default 64 [ 0.564143] hw perfevents: enabled with armv8_cortex_a72 PMU driver, 7 counters available [ 0.573215] Initialise system trusted keyrings [ 0.577887] workingset: timestamp_bits=46 max_order=20 bucket_order=0 [ 0.586573] squashfs: version 4.0 (2009/01/31) Phillip Lougher [ 0.592853] NFS: Registering the id_resolver key type [ 0.598038] Key type id_resolver registered [ 0.602310] Key type id_legacy registered [ 0.606431] nfs4filelayout_init: NFSv4 File Layout Driver Registering... [ 0.613281] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering... [ 0.639878] Key type asymmetric registered [ 0.644063] Asymmetric key parser 'x509' registered [ 0.649073] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245) [ 0.656721] io scheduler mq-deadline registered [ 0.661350] io scheduler kyber registered [ 0.667214] pinctrl-single 4301c000.pinctrl: 13 pins, size 52 [ 0.673203] pinctrl-single 4301c038.pinctrl: 2 pins, size 8 [ 0.679003] pinctrl-single 4301c068.pinctrl: 59 pins, size 236 [ 0.685200] pinctrl-single 4301c174.pinctrl: 8 pins, size 32 [ 0.691159] pinctrl-single 11c000.pinctrl: 67 pins, size 268 [ 0.697162] pinctrl-single 11c11c.pinctrl: 3 pins, size 12 [ 0.703216] pinctrl-single a40000.pinctrl: 512 pins, size 2048 [ 0.712257] Serial: 8250/16550 driver, 12 ports, IRQ sharing enabled [ 0.723217] loop: module loaded [ 0.726988] megasas: 07.719.03.00-rc1 [ 0.732176] tun: Universal TUN/TAP device driver, 1.6 [ 0.737714] VFIO - User Level meta-driver version: 0.3 [ 0.743343] usbcore: registered new interface driver usb-storage [ 0.749818] i2c_dev: i2c /dev entries driver [ 0.754764] sdhci: Secure Digital Host Controller Interface driver [ 0.761098] sdhci: Copyright(c) Pierre Ossman [ 0.765652] sdhci-pltfm: SDHCI platform and OF driver helper [ 0.771690] ledtrig-cpu: registered to indicate activity on CPUs [ 0.777914] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping .... [ 0.784626] usbcore: registered new interface driver usbhid [ 0.790322] usbhid: USB HID core driver [ 0.794727] optee: probing for conduit method. I/TC: Reserved shared memory is enabled I/TC: Dynamic shared memory is enabled I/TC: Normal World virtualization support is disabled I/TC: Asynchronous notifications are disabled [ 0.799290] optee: revision 4.1 (012cdca4) [ 0.815718] optee: dynamic shared memory is enabled [ 0.825105] optee: initialized driver [ 0.829912] Initializing XFRM netlink socket [ 0.834303] NET: Registered PF_PACKET protocol family [ 0.839497] Key type dns_resolver registered [ 0.844055] registered taskstats version 1 [ 0.848257] Loading compiled-in X.509 certificates [ 0.859283] ti-sci 44083000.system-controller: ABI: 3.1 (firmware rev 0x0009 '9.2.4--v09.02.04 (Kool Koala)') [ 0.887753] omap_i2c 42120000.i2c: bus 0 rev0.12 at 400 kHz [ 0.894248] pca953x 1-0021: supply vcc not found, using dummy regulator [ 0.901093] pca953x 1-0021: using no AI [ 0.929135] pca953x 1-0020: supply vcc not found, using dummy regulator [ 0.935948] pca953x 1-0020: using no AI [ 0.940511] pca953x 1-0022: supply vcc not found, using dummy regulator [ 0.947317] pca953x 1-0022: using AI [ 0.951597] omap_i2c 2000000.i2c: bus 1 rev0.12 at 400 kHz [ 0.957747] pca953x 2-0020: supply vcc not found, using dummy regulator [ 0.964576] pca953x 2-0020: using no AI [ 0.989028] omap_i2c 2010000.i2c: bus 2 rev0.12 at 400 kHz [ 0.994803] ti-sci-intr 42200000.interrupt-controller: Interrupt Router 137 domain created [ 1.003339] ti-sci-intr bus@100000:interrupt-controller@a00000: Interrupt Router 131 domain created [ 1.012669] ti-sci-intr 310e0000.interrupt-controller: Interrupt Router 213 domain created [ 1.021264] ti-sci-inta 33d00000.msi-controller: Interrupt Aggregator domain 209 created [ 1.030911] k3-ringacc 2b800000.ringacc: Ring Accelerator probed rings:286, gp-rings[96,32] sci-dev-id:235 [ 1.040804] k3-ringacc 2b800000.ringacc: dma-ring-reset-quirk: disabled [ 1.047565] k3-ringacc 2b800000.ringacc: RA Proxy rev. 66349100, num_proxies:64 [ 1.057280] k3-ringacc 3c000000.ringacc: Ring Accelerator probed rings:1024, gp-rings[120,200] sci-dev-id:211 [ 1.067436] k3-ringacc 3c000000.ringacc: dma-ring-reset-quirk: disabled [ 1.074197] k3-ringacc 3c000000.ringacc: RA Proxy rev. 66349100, num_proxies:64 [ 1.082173] 40a00000.serial: ttyS1 at MMIO 0x40a00000 (irq = 251, base_baud = 6000000) is a 8250 [ 1.091666] 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 252, base_baud = 3000000) is a 8250 [ 1.100519] printk: console [ttyS2] enabled [ 1.100519] printk: console [ttyS2] enabled [ 1.108960] printk: bootconsole [ns16550a0] disabled [ 1.108960] printk: bootconsole [ns16550a0] disabled [ 1.119390] 2810000.serial: ttyS3 at MMIO 0x2810000 (irq = 253, base_baud = 3000000) is a 8250 [ 1.129203] davinci_mdio 46000f00.mdio: Configuring MDIO in manual mode [ 1.172728] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000 [ 1.181564] davinci_mdio 46000f00.mdio: phy[0]: device 46000f00.mdio:00, driver TI DP83867 [ 1.189840] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA02102, cpsw version 0x6BA82102 Ports: 2 quirks:00000000 [ 1.202680] am65-cpsw-nuss 46000000.ethernet: initialized cpsw ale version 1.4 [ 1.209889] am65-cpsw-nuss 46000000.ethernet: ALE Table size 64 [ 1.216067] pps pps0: new PPS source ptp0 [ 1.220217] am65-cpsw-nuss 46000000.ethernet: CPTS ver 0x4e8a010b, freq:500000000, add_val:1 pps:1 [ 1.230508] am65-cpts 310d0000.cpts: CPTS ver 0x4e8a010b, freq:200000000, add_val:4 pps:0 [ 1.242009] gpio-mux mux-controller: 2-way mux-controller registered [ 1.248471] mmc0: CQHCI version 5.10 [ 1.289273] mmc0: SDHCI controller on 4f80000.mmc [4f80000.mmc] using ADMA 64-bit [ 1.384040] mmc0: Command Queue Engine enabled [ 1.388550] mmc0: new HS400 MMC card at address 0001 [ 1.394225] mmcblk0: mmc0:0001 G1M15L 29.6 GiB [ 1.400373] mmcblk0boot0: mmc0:0001 G1M15L 31.5 MiB [ 1.406474] mmcblk0boot1: mmc0:0001 G1M15L 31.5 MiB [ 1.412614] mmcblk0rpmb: mmc0:0001 G1M15L 4.00 MiB, chardev (240:0) [ 1.497291] tps6594-rtc tps6594-rtc.4.auto: registered as rtc0 [ 1.504063] tps6594-rtc tps6594-rtc.4.auto: setting system clock to 2022-04-30T08:44:08 UTC (1651308248) [ 1.667378] omap-mailbox 31f80000.mailbox: omap mailbox rev 0x66fc8900 [ 1.674377] omap-mailbox 31f81000.mailbox: omap mailbox rev 0x66fc8900 [ 1.683313] ti-udma 285c0000.dma-controller: Channels: 26 (tchan: 13, rchan: 13, gp-rflow: 8) [ 1.694835] ti-udma 31150000.dma-controller: Channels: 50 (tchan: 25, rchan: 25, gp-rflow: 8) [ 1.709292] spi-nor spi0.0: s28hs512t (65536 Kbytes) [ 1.714365] 7 fixed-partitions partitions found on MTD device 47040000.spi.0 [ 1.721480] Creating 7 MTD partitions on "47040000.spi.0": [ 1.726996] 0x000000000000-0x000000100000 : "ospi.tiboot3" [ 1.733505] 0x000000100000-0x000000300000 : "ospi.tispl" [ 1.739637] 0x000000300000-0x000000700000 : "ospi.u-boot" [ 1.745894] 0x000000700000-0x000000740000 : "ospi.env" [ 1.751830] 0x000000740000-0x000000780000 : "ospi.env.backup" [ 1.758367] 0x000000800000-0x000003fc0000 : "ospi.rootfs" [ 1.764567] 0x000003fc0000-0x000004000000 : "ospi.phypattern" [ 1.775985] davinci_mdio 46000f00.mdio: Configuring MDIO in manual mode [ 1.820736] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000 [ 1.829731] davinci_mdio 46000f00.mdio: phy[0]: device 46000f00.mdio:00, driver TI DP83867 [ 1.838009] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA02102, cpsw version 0x6BA82102 Ports: 2 quirks:00000000 [ 1.850878] am65-cpsw-nuss 46000000.ethernet: initialized cpsw ale version 1.4 [ 1.858105] am65-cpsw-nuss 46000000.ethernet: ALE Table size 64 [ 1.865341] pps pps0: new PPS source ptp1 [ 1.869487] am65-cpsw-nuss 46000000.ethernet: CPTS ver 0x4e8a010b, freq:500000000, add_val:1 pps:1 [ 1.880669] am65-cpsw-nuss 46000000.ethernet: set new flow-id-base 48 [ 1.889859] debugfs: Directory 'pd:240' with parent 'pm_genpd' already present! [ 1.889859] mmc1: CQHCI version 5.10 [ 1.903942] ALSA device list: [ 1.906940] No soundcards found. [ 1.941891] mmc1: SDHCI controller on 4fb0000.mmc [4fb0000.mmc] using ADMA 64-bit [ 1.949544] Waiting for root device PARTUUID=164f123c-02... [ 2.008815] mmc1: new ultra high speed SDR104 SDHC card at address aaaa [ 2.016173] mmcblk1: mmc1:aaaa SC16G 14.8 GiB [ 2.025238] mmcblk1: p1 p2 [ 2.068522] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Quota mode: none. [ 2.077098] VFS: Mounted root (ext4 filesystem) on device 179:98. [ 2.086878] devtmpfs: mounted [ 2.091206] Freeing unused kernel memory: 1984K [ 2.095856] Run /sbin/init as init process [ 2.307430] NET: Registered PF_INET6 protocol family [ 2.313461] Segment Routing with IPv6 [ 2.317155] In-situ OAM (IOAM) with IPv6 [ 2.345142] systemd[1]: systemd 250.5+ running in system mode (+PAM -AUDIT -SELINUX -APPARMOR +IMA -SMACK +SECCOMP -GCRYPT -GNUTLS -OPENSSL +ACL +BLKID -CURL -ELFUTILS -FIDO2 -IDN2 -IDN -IPTC +KMOD -LIBCRYPTSETUP +LIBFDISK -PCRE2 -PWQUALITY -P11KIT -QRENCODE -BZIP2 -LZ4 -XZ -ZLIB +ZSTD -BPF_FRAMEWORK -XKBCOMMON +UTMP +SYSVINIT default-hierarchy=hybrid) [ 2.376845] systemd[1]: Detected architecture arm64. Welcome to Arago 2023.10! [ 2.439545] systemd[1]: Hostname set to <j7200-evm>. [ 2.525131] systemd-sysv-generator[148]: SysV service '/etc/init.d/thermal-zone-init' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust. [ 2.766220] systemd[1]: /lib/systemd/system/bt-enable.service:9: Standard output type syslog is obsolete, automatically updating to journal. Please update your unit file, and consider removing the setting altogether. [ 2.817303] systemd[1]: /etc/systemd/system/sync-clocks.service:11: Standard output type syslog is obsolete, automatically updating to journal. Please update your unit file, and consider removing the setting altogether. [ 2.872591] systemd[1]: Queued start job for default target Graphical Interface. [ 2.920503] systemd[1]: Created slice Slice /system/getty. [ OK ] Created slice Slice /system/getty. [ 2.942427] systemd[1]: Created slice Slice /system/modprobe. [ OK ] Created slice Slice /system/modprobe. [ 2.967721] systemd[1]: Created slice Slice /system/serial-getty. [ OK ] Created slice Slice /system/serial-getty. [ 2.990636] systemd[1]: Created slice User and Session Slice. [ OK ] Created slice User and Session Slice. [ 3.012986] systemd[1]: Started Dispatch Password Requests to Console Directory Watch. [ OK ] Started Dispatch Password …ts to Console Directory Watch. [ 3.036979] systemd[1]: Started Forward Password Requests to Wall Directory Watch. [ OK ] Started Forward Password R…uests to Wall Directory Watch. [ 3.061159] systemd[1]: Reached target Path Units. [ OK ] Reached target Path Units. [ 3.076891] systemd[1]: Reached target Remote File Systems. [ OK ] Reached target Remote File Systems. [ 3.096870] systemd[1]: Reached target Slice Units. [ OK ] Reached target Slice Units. [ 3.112878] systemd[1]: Reached target Swaps. [ OK ] Reached target Swaps. [ 3.168204] systemd[1]: Listening on RPCbind Server Activation Socket. [ OK ] Listening on RPCbind Server Activation Socket. [ 3.192972] systemd[1]: Reached target RPC Port Mapper. [ OK ] Reached target RPC Port Mapper. [ 3.221232] systemd[1]: Listening on Process Core Dump Socket. [ OK ] Listening on Process Core Dump Socket. [ 3.245159] systemd[1]: Listening on initctl Compatibility Named Pipe. [ OK ] Listening on initctl Compatibility Named Pipe. [ 3.269501] systemd[1]: Listening on Journal Audit Socket. [ OK ] Listening on Journal Audit Socket. [ 3.293308] systemd[1]: Listening on Journal Socket (/dev/log). [ OK ] Listening on Journal Socket (/dev/log). [ 3.317385] systemd[1]: Listening on Journal Socket. [ OK ] Listening on Journal Socket. [ 3.333511] systemd[1]: Listening on Network Service Netlink Socket. [ OK ] Listening on Network Service Netlink Socket. [ 3.357435] systemd[1]: Listening on udev Control Socket. [ OK ] Listening on udev Control Socket. [ 3.377214] systemd[1]: Listening on udev Kernel Socket. [ OK ] Listening on udev Kernel Socket. [ 3.397264] systemd[1]: Listening on User Database Manager Socket. [ OK ] Listening on User Database Manager Socket. [ 3.445136] systemd[1]: Mounting Huge Pages File System... Mounting Huge Pages File System... [ 3.463781] systemd[1]: Mounting POSIX Message Queue File System... Mounting POSIX Message Queue File System... [ 3.513145] systemd[1]: Mounting Kernel Debug File System... Mounting Kernel Debug File System... [ 3.533269] systemd[1]: Kernel Trace File System was skipped because of a failed condition check (ConditionPathExists=/sys/kernel/tracing). [ 3.553521] systemd[1]: Mounting Temporary Directory /tmp... Mounting Temporary Directory /tmp... [ 3.578751] systemd[1]: Starting Create List of Static Device Nodes... Starting Create List of Static Device Nodes... [ 3.605402] systemd[1]: Starting Load Kernel Module configfs... Starting Load Kernel Module configfs... [ 3.633266] systemd[1]: Starting Load Kernel Module drm... Starting Load Kernel Module drm... [ 3.657150] systemd[1]: Starting Load Kernel Module fuse... Starting Load Kernel Module fuse... [ 3.670010] fuse: init (API version 7.37) [ 3.683670] systemd[1]: Starting RPC Bind... Starting RPC Bind... [ 3.701001] systemd[1]: File System Check on Root Device was skipped because of a failed condition check (ConditionPathIsReadWrite=!/). [ 3.718047] systemd[1]: Starting Journal Service... Starting Journal Service... [ 3.761283] systemd[1]: Starting Load Kernel Modules... Starting Load Kernel Modules... [ 3.777841] systemd[1]: Starting Generate network units from Kernel command line... Starting Generate network …ts from Kernel command line... [ 3.796292] cryptodev: loading out-of-tree module taints kernel. [ 3.803127] cryptodev: driver 1.12 loaded. [ 3.811368] systemd[1]: Starting Remount Root and Kernel File Systems... Starting Remount Root and Kernel File Systems... [ 3.828119] EXT4-fs (mmcblk1p2): re-mounted. Quota mode: none. [ 3.849694] systemd[1]: Starting Coldplug All udev Devices... Starting Coldplug All udev Devices... [ 3.883165] systemd[1]: Started RPC Bind. [ OK ] Started RPC Bind. [ 3.901783] systemd[1]: Started Journal Service. [ OK ] Started Journal Service. [ OK ] Mounted Huge Pages File System. [ OK ] Mounted POSIX Message Queue File System. [ OK ] Mounted Kernel Debug File System. [ OK ] Mounted Temporary Directory /tmp. [ OK ] Finished Create List of Static Device Nodes. [ OK ] Finished Load Kernel Module configfs. [ OK ] Finished Load Kernel Module drm. [ OK ] Finished Load Kernel Module fuse. [ OK ] Finished Load Kernel Modules. [ OK ] Finished Generate network units from Kernel command line. [ OK ] Finished Remount Root and Kernel File Systems. Mounting NFSD configuration filesystem... Mounting FUSE Control File System... Mounting Kernel Configuration File System... Starting Flush Journal to Persistent Storage... [ 4.211158] systemd-journald[163]: Received client request to flush runtime journal. Starting Apply Kernel Variables... Starting Create Static Device Nodes in /dev... [FAILED] Failed to mount NFSD configuration filesystem. See 'systemctl status proc-fs-nfsd.mount' for details. [DEPEND] Dependency failed for NFS server and services. [DEPEND] Dependency failed for NFS Mount Daemon. [ OK ] Mounted FUSE Control File System. [ OK ] Mounted Kernel Configuration File System. [ OK ] Finished Flush Journal to Persistent Storage. [ OK ] Finished Coldplug All udev Devices. [ OK ] Finished Apply Kernel Variables. [ OK ] Finished Create Static Device Nodes in /dev. [ OK ] Reached target Preparation for Local File Systems. Mounting /media/ram... Mounting /var/volatile... [ 4.505936] audit: type=1334 audit(1651308251.500:2): prog-id=5 op=LOAD [ 4.513155] audit: type=1334 audit(1651308251.504:3): prog-id=6 op=LOAD Starting Rule-based Manage…for Device Events and Files... [ OK ] Mounted /media/ram. [ OK ] Mounted /var/volatile. Starting Load/Save Random Seed... [ OK ] Reached target Local File Systems. Starting Create Volatile Files and Directories... [ OK ] Started Rule-based Manager for Device Events and Files. [ OK ] Finished Create Volatile Files and Directories. Starting Network Time Synchronization... Starting Record System Boot/Shutdown in UTMP... [ OK ] Finished Record System Boot/Shutdown in UTMP. [ OK ] Started Network Time Synchronization. [ OK ] Reached target System Initialization. [ OK ] Started Daily Cleanup of Temporary Directories. [ OK ] Reached target System Time Set. [ OK ] Started Daily rotation of log files. [ OK ] Reached target Timer Units. [ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket. [ 5.048113] random: crng init done [ OK ] Listening on D-Bus System Message Bus Socket. Starting Docker Socket for the API...[ 5.079475] CAN device driver interface [ OK ] Listening on dropbear.socket. [ OK ] Listening on PC/SC Smart Card Daemo[ 5.124355] j721e-pcie-host 2910000.pcie: host bridge /bus@100000/pcie@2910000 ranges: n Activation Socket. Starting Weston socket... Starting D-Bus System Message Bus... Starting Reboot and dump vmcore via kexec... [ OK ] Finished Load/Save Random Seed. [ 5.208573] ti-udma 285c0000.dma-controller: chan1: is running! [ 5.214568] j721e-pcie-host 2910000.pcie: IO 0x0018001000..0x0018010fff -> 0x0018001000 [ OK ] Listening on Docker Socket for the API. [ OK ] Listening on Weston socket. [ 5.249397] j721e-pcie-host 2910000.pcie: MEM 0x0018011000..0x001fffffff -> 0x0018011000 [ OK ] Finished Reboot and dump vmcore via kexec. [ 5.268934] j721e-pcie-host 2910000.pcie: IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000 [ OK ] Found device /dev/ttyS2. [ OK ] Started D-Bus System Message Bus. [ OK ] Reached target Socket Units. [ OK ] Reached target Basic System. [ OK ] Started Job spooling tools. [ OK ] Started Periodic Command Scheduler. Starting DEMO... Starting Print notice about GPLv3 packages... Starting IPv6 Packet Filtering Framework... Starting IPv4 Packet Filtering Framework... [ OK ] Started irqbalance daemon. Starting Telephony service... Starting Expand the rootfs…ll size of the boot device.... [ OK ] Started strongSwan IPsec I…IKEv2 [ 5.549473] audit: type=1334 audit(1651308252.544:4): prog-id=7 op=LOAD daemon using ipsec.conf. Starting User Login Management... [ 5.564777] audit: type=1334 audit(1651308252.552:5): prog-id=8 op=LOAD [ OK ] Started TEE Supplicant. Starting Telnet Server... [ OK ] Finished IPv4 Packet Filtering Framework. [ 5.599351] platform 41000000.r5f: R5F core may have been powered on by a different host, programmed state (0) != actual state (1) [ OK ] Finished IPv6 Packet Filtering Framework. [ OK ] Reached target Preparation for Network. Starting Network Configuration... [ OK ] Finished Telnet Server. [ OK ] Started DEMO. [ OK ] Started Telephony service. [ 5.771769] platform 41000000.r5f: configured R5F for IPC-only mode [ 5.804340] platform 41000000.r5f: assigned reserved memory node r5f-dma-memory@a0000000 [ 5.827974] remoteproc remoteproc0: 41000000.r5f is available [ 5.866563] Bluetooth: Core ver 2.22 [ 5.872623] NET: Registered PF_BLUETOOTH protocol family [ 5.883029] Bluetooth: HCI device and connection manager initialized [ 5.892405] Bluetooth: HCI socket layer initialized [ 5.898114] remoteproc remoteproc0: attaching to 41000000.r5f [ 5.900631] Bluetooth: L2CAP socket layer initialized [ 5.915957] Bluetooth: SCO socket layer initialized [ OK ] Finished Expand the rootfs…full size of the boot device.. [ 5.993220] platform 41000000.r5f: R5F core initialized in IPC-only mode [ 6.000071] rproc-virtio rproc-virtio.10.auto: assigned reserved memory node r5f-dma-memory@a0000000 [ 6.018575] virtio_rpmsg_bus virtio0: rpmsg host is online [ 6.026564] virtio_rpmsg_bus virtio0: creating channel ti.ipc4.ping-pong addr 0xd [ 6.029644] rproc-virtio rproc-virtio.10.auto: registered virtio0 (type 7) [ 6.040847] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0xe [ 6.041016] remoteproc remoteproc0: remote processor 41000000.r5f is now attached [ OK ] Started User Login Management. [ 6.134927] platform 41400000.r5f: R5F core may have been powered on by a different host, programmed state (0) != actual state (1) [ 6.144369] cfg80211: Loading compiled-in X.509 certificates for regulatory database [ 6.154588] platform 41400000.r5f: configured R5F for IPC-only mode [ 6.162629] m_can_platform 2701000.can: m_can device registered (irq=684, version=32) [ 6.163081] platform 41400000.r5f: assigned reserved memory node r5f-dma-memory@a1000000 [ 6.177858] m_can_platform 2731000.can: m_can device registered (irq=685, version=32) [ 6.180659] remoteproc remoteproc1: 41400000.r5f is available [ 6.193184] remoteproc remoteproc1: attaching to 41400000.r5f [ 6.198146] m_can_platform 40528000.can: m_can device registered (irq=686, version=32) [ 6.201349] platform 41400000.r5f: R5F core initialized in IPC-only mode [ 6.214414] rproc-virtio rproc-virtio.11.auto: assigned reserved memory node r5f-dma-memory@a1000000 [ 6.217272] m_can_platform 40568000.can: m_can device registered (irq=687, version=32) [ 6.223952] virtio_rpmsg_bus virtio1: rpmsg host is online [ 6.233682] virtio_rpmsg_bus virtio1: creating channel ti.ipc4.ping-pong addr 0xd [ 6.237513] rproc-virtio rproc-virtio.11.auto: registered virtio1 (type 7) [ 6.251495] remoteproc remoteproc1: remote processor 41400000.r5f is now attached [ 6.254534] virtio_rpmsg_bus virtio1: creating channel rpmsg_chrdev addr 0xe [ 6.282811] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7' [ 6.290896] cfg80211: Loaded X.509 cert 'wens: 61c038651aabdcf94bd0ac7ff06c7248db18c600' [ 6.322501] platform 5c00000.r5f: configured R5F for IPC-only mode [ OK ] Started Network Configuration. [ 6.424377] platform 5c00000.r5f: assigned reserved memory node r5f-dma-memory@a2000000 Starting Network Name Resolution... [ 6.448552] am65-cpsw-nuss 46000000.ethernet eth0: PHY [46000f00.mdio:00] driver [TI DP83867] (irq=POLL) [ 6.465745] am65-cpsw-nuss 46000000.ethernet eth0: configuring for phy/rgmii-rxid link mode [ 6.472905] j721e-pcie-host 2910000.pcie: PCI host bridge to bus 0000:00 [ 6.527828] pci_bus 0000:00: root bus resource [bus 00-ff] [ 6.533597] pci_bus 0000:00: root bus resource [io 0x0000-0xffff] (bus address [0x18001000-0x18010fff]) [ 6.543333] pci_bus 0000:00: root bus resource [mem 0x18011000-0x1fffffff] [ 6.555046] pci 0000:00:00.0: [104c:b00f] type 01 class 0x060400 [ 6.570188] pci 0000:00:00.0: supports D1 [ 6.580044] pci 0000:00:00.0: PME# supported from D0 D1 D3hot [ 6.668097] pci 0000:00:00.0: reg 0x224: [mem 0x00000000-0x003fffff 64bit] [ 6.721390] remoteproc remoteproc2: 5c00000.r5f is available [ 6.835233] pci 0000:00:00.0: VF(n) BAR0 space: [mem 0x00000000-0x00ffffff 64bit] (contains BAR0 for 4 VFs) [ 6.849623] remoteproc remoteproc2: attaching to 5c00000.r5f [ 6.856280] platform 5c00000.r5f: R5F core initialized in IPC-only mode [ 6.863716] rproc-virtio rproc-virtio.12.auto: assigned reserved memory node r5f-dma-memory@a2000000 [ 6.905549] pci 0000:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring [ 6.917028] pci_bus 0000:01: busn_res: [bus 01-ff] end is updated to 01 [ 6.924032] pci 0000:00:00.0: BAR 7: assigned [mem 0x18400000-0x193fffff 64bit] [ 6.931680] pci 0000:00:00.0: PCI bridge to [bus 01] [ 6.938060] pcieport 0000:00:00.0: PME: Signaling with IRQ 689 [ 6.945028] virtio_rpmsg_bus virtio2: rpmsg host is online [ OK ] Started Network Name Resolution[ 6.952909] virtio_rpmsg_bus virtio2: creating channel ti.ethfw.ethdevice addr 0x65 . [ OK ] Reached target Network. [ 6.964533] pcieport 0000:00:00.0: AER: enabled with IRQ 689 0;32m OK ] Reached target Host and Network Name L[ 6.975273] virtio_rpmsg_bus virtio2: creating channel rpmsg_chrdev addr 0x15 ookups. [ 7.004710] rproc-virtio rproc-virtio.12.auto: registered virtio2 (type 7) [ 7.012416] remoteproc remoteproc2: remote processor 5c00000.r5f is now attached [ 7.013735] platform 5d00000.r5f: configured R5F for IPC-only mode [ 7.013905] platform 5d00000.r5f: assigned reserved memory node r5f-dma-memory@a3000000 [ 7.048978] remoteproc remoteproc3: 5d00000.r5f is available Starting Avahi mDNS/DNS-SD Stack... Starting Enable and configure wl18xx bluetooth stack... Starting containerd container runtime... [ OK ] Started Netperf Benchmark Server. [ OK ] Started NFS status monitor for NFSv2/3 locking.. Starting Simple Network Ma…ent Protocol (SNMP) Daemon.... Starting Simple Network Ma…rotocol (SNMP) Trap Daemon.... Starting Permit User Sessions... [ 7.133083] remoteproc remoteproc3: attaching to 5d00000.r5f [ 7.155203] platform 5d00000.r5f: R5F core initialized in IPC-only mode [ OK ] Listening on Load/Save RF …itch S[ 7.161959] rproc-virtio rproc-virtio.13.auto: assigned reserved memory node r5f-dma-memory@a3000000 tatus /dev/rfkill Watch. [ OK ] Started Avahi mDNS/DNS-SD Stack. [ OK ] Finished Permit User Sessions 7.188341] virtio_rpmsg_bus virtio3: rpmsg host is online m. [ 7.196687] rproc-virtio rproc-virtio.13.auto: registered virtio3 (type 7) [ 7.202026] virtio_rpmsg_bus virtio3: creating channel ti.ipc4.ping-pong addr 0xd [ 7.203702] remoteproc remoteproc3: remote processor 5d00000.r5f is now attached [ 7.214405] virtio_rpmsg_bus virtio3: creating channel rpmsg_chrdev addr 0xe [ OK ] Started Getty on tty1. [ OK ] Started Serial Getty on ttyS2. [ OK ] Reached target Login Prompts. Starting Synchronize System and HW clocks... Starting Weston, a Wayland…ositor, as a system service... [ OK ] Finished Enable and configure wl18xx bluetooth stack. [ 7.341637] m_can_platform 2731000.can main_mcan3: renamed from can1 [ 7.404200] audit: type=1334 audit(1651308254.396:6): prog-id=9 op=LOAD [ 7.412988] audit: type=1334 audit(1651308254.408:7): prog-id=10 op=LOAD Starting User Database Manager... [ 7.466220] m_can_platform 40528000.can mcu_mcan0: renamed from can2 [ 7.519104] m_can_platform 40568000.can mcu_mcan1: renamed from can3 [ 7.564434] m_can_platform 2701000.can main_mcan0: renamed from can0 [ OK ] Started User Database Manager. [ 7.635841] ti_cpsw_proxy_client virtio2.ti.ethfw.ethdevice.-1.101: 1 Virtual Switch Port(s), 1 Virtual MAC Only Port(s) [ OK ] Created slice User Slice of UID 1000. [ 7.691091] ti_cpsw_proxy_client virtio2.ti.ethfw.ethdevice.-1.101: Virt Port: 0, Type: Switch Port, Iface: eth1, Num TX: 2, Num RX: 1, Token: 0 [ 7.704754] ti_cpsw_proxy_client virtio2.ti.ethfw.ethdevice.-1.101: Virt Port: 4, Type: MAC Port, Iface: eth2, Num TX: 1, Num RX: 1, Token: 400 Starting User Runtime Directory /run/user/1000... [ OK ] Finished User Runtime Directory /run/user/1000. Starting User Manager for UID 1000... [ 7.766243] audit: type=1006 audit(1651308254.760:8): pid=562 uid=0 old-auid=4294967295 auid=1000 tty=(none) old-ses=4294967295 ses=1 res=1 [ 7.785081] audit: type=1300 audit(1651308254.760:8): arch=c00000b7 syscall=64 success=yes exit=4 a0=8 a1=ffffcbc0b808 a2=4 a3=ffff9c9ae020 items=0 ppid=1 pid=562 auid=1000 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=1 comm="(systemd)" exe="/lib/systemd/systemd" key=(null) [ 7.833627] audit: type=1327 audit(1651308254.760:8): proctitle="(systemd)" [ OK ] Started Simple Network Man… Protocol (SNMP) Trap Daemon.. [ OK ] Finished Synchronize System and HW clocks. [ 8.070983] ti_cpsw_proxy_client virtio2.ti.ethfw.ethdevice.-1.101: started virt port: 4 on interface eth2 [ 8.126009] ti_cpsw_proxy_client virtio2.ti.ethfw.ethdevice.-1.101: started virt port: 0 on interface eth1 [ OK ] Started Simple Network Man…ement Protocol (SNMP) Daemon.. [ OK ] Started User Manager for UID 1000. [ OK ] Started Session c1 of User weston. [ 8.294058] audit: type=1006 audit(1651308255.288:9): pid=513 uid=0 old-auid=4294967295 auid=1000 tty=tty7 old-ses=4294967295 ses=2 res=1 [ 8.306483] audit: type=1300 audit(1651308255.288:9): arch=c00000b7 syscall=64 success=yes exit=4 a0=8 a1=ffffcbc0b808 a2=4 a3=ffff9c9ae020 items=0 ppid=1 pid=513 auid=1000 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=tty7 ses=2 comm="(weston)" exe="/lib/systemd/systemd" key=(null) [ 8.332758] audit: type=1327 audit(1651308255.288:9): proctitle="(weston)" [FAILED] Failed to start Weston, a …mpositor, as a system service. See 'systemctl status weston.service' for details. [ OK ] Created slice Slice /system/systemd-fsck. [ OK ] Found device /dev/mmcblk1p1. Starting File System Check on /dev/mmcblk1p1... [ OK ] Started containerd container runtime. [ OK ] Finished File System Check on /dev/mmcblk1p1. Mounting /run/media/boot-mmcblk1p1... [ OK ] Mounted /run/media/boot-mmcblk1p1. *************************************************************** *************************************************************** NOTICE: This file system contains the following GPL-3.0 packages: adwaita-icon-theme-symbolic autoconf-dev autoconf bash-dev bash bc-dev bc binutils-dev binutils ccache-dev ccache cifs-utils-dev cifs-utils coreutils-dev coreutils-stdbuf coreutils cpio-dev cpio cpp-symlinks cpp diffutils-dev diffutils dosfstools-dev dosfstools elfutils-dev elfutils findutils-dev findutils g++-symlinks g++ gawk-dev gawk gcc-dev gcc-symlinks gcc gdb-dev gdb gdbserver gettext-dev gettext glmark2-dev glmark2 gnu-config grep-dev grep grub-common grub-dev grub-editenv grub-efi-dev grub-efi grub gzip-dev gzip hidapi-dev hidapi less-dev less libasm1 libatomic-dev libatomic1 libbfd libdebuginfod1 libdw1 libeigen-dev libelf1 libgcc-s-dev libgcc1 libgdbm-compat4 libgdbm-dev libgdbm6 libgettextlib libgettextsrc libgmp-dev libgmp10 libgmpxx4 libgomp-dev libgomp1 libidn2-0 libidn2-dev libmpc-dev libmpc3 libmpfr-dev libmpfr6 libopcodes libqt5charts-dev libqt5charts-examples libqt5charts-mkspecs libqt5charts-plugins libqt5charts-qmldesigner libqt5charts-qmlplugins libqt5charts5 libqt5sensors-dev libqt5sensors-mkspecs libqt5sensors-plugins libqt5sensors-qmlplugins libqt5sensors5 libqt5serialport-dev libqt5serialport-examples libqt5serialport-mkspecs libqt5serialport-plugins libqt5serialport-qmlplugins libqt5serialport5 libqt5svg-dev libqt5svg-examples libqt5svg-mkspecs libqt5svg-plugins libqt5svg-qmlplugins libqt5svg5 libqt5virtualkeyboard-dev libqt5virtualkeyboard-mkspecs libqt5virtualkeyboard-plugins libqt5virtualkeyboard-qmlplugins libqt5virtualkeyboard5 libqt5webchannel-dev libqt5webchannel-mkspecs libqt5webchannel-plugins libqt5webchannel-qmlplugins libqt5webchannel5 libqt5websockets-dev libqt5websockets-mkspecs libqt5websockets-plugins libqt5websockets-qmlplugins libqt5websockets5 libqt5xmlpatterns-dev libqt5xmlpatterns-mkspecs libqt5xmlpatterns-plugins libqt5xmlpatterns-qmlplugins libqt5xmlpatterns5 libreadline-dev libreadline8 libstdc++-dev libstdc++6 libtalloc-dev libtalloc libunistring-dev libunistring2 m4-dev m4 make-dev make nettle-dev nettle parted-dev parted patch-dev patch piglit-dev piglit python3-can-dev python3-can qt3d-dev qt3d-mkspecs qt3d-plugins qt3d-qmlplugins qt3d qtbase-dev qtbase-examples qtbase-mkspecs qtbase-plugins qtbase-qmlplugins qtbase qtconnectivity-dev qtconnectivity-mkspecs qtconnectivity-plugins qtconnectivity-qmlplugins qtconnectivity qtdeclarative-dev qtdeclarative-mkspecs qtdeclarative-plugins qtdeclarative-qmlplugins qtdeclarative-tools qtdeclarative qtgraphicaleffects-dev qtgraphicaleffects-mkspecs qtgraphicaleffects-plugins qtgraphicaleffects-qmlplugins qtgraphicaleffects qtlocation-dev qtlocation-examples qtlocation-mkspecs qtlocation-plugins qtlocation-qmlplugins qtlocation qtmultimedia-dev qtmultimedia-examples qtmultimedia-mkspecs qtmultimedia-plugins qtmultimedia-qmlplugins qtmultimedia qtquics-dev.control qtquics-mkspecs.control qtquics-plugins.control qtquics-qmldesigner.control qtquics-qmlplugins.control qtquics.control qtquics2-dev.control qtquics2-mkspecs.control qtquics2-plugins.control qtquics2-qmldesigner.control qtquics2-qmlplugins.control qtquics2.control qtscript-dev qtscript-examples qtscript-mkspecs qtscript-plugins qtscript-qmlplugins qtscript qtwayland-dev qtwayland-examples qtwayland-mkspecs qtwayland-plugins qtwayland-qmlplugins qtwayland tar-dev tar usbutils-dev which-dev which If you do not wish to distribute GPL-3.0 components please remove the above packages prior to distribution. This can be done using the opkg remove command. i.e.: opkg remove <package> Where <package> is the name printed in the list above NOTE: If the package is a dependency of another package you will be notified of the dependent packages. You should use the --force-removal-of-dependent-packages option to also remove the dependent packages as well *************************************************************** *************************************************************** [ OK ] Finished Print notice about GPLv3 packages. [ OK ] Reached target Multi-User System. [ OK ] Reached target Graphical Interface. Starting Record Runlevel Change in UTMP... [ OK ] Finished Record Runlevel Change in UTMP. _____ _____ _ _ | _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_ | | _| .'| . | . | | __| _| . | | | -_| _| _| |__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_| |___| |___| Arago Project j7200-evm - Arago 2023.10 j7200-evm -
Jai,
[ 0.887753] omap_i2c 42120000.i2c: bus 0 rev0.12 at 400 kHz
[ 0.894248] pca953x 1-0021: supply vcc not found, using dummy regulator
[ 0.901093] pca953x 1-0021: using no AI
[ 0.929135] pca953x 1-0020: supply vcc not found, using dummy regulator
[ 0.935948] pca953x 1-0020: using no AI
[ 0.940511] pca953x 1-0022: supply vcc not found, using dummy regulator
[ 0.947317] pca953x 1-0022: using AI
[ 0.951597] omap_i2c 2000000.i2c: bus 1 rev0.12 at 400 kHz
[ 0.957747] pca953x 2-0020: supply vcc not found, using dummy regulator
[ 0.964576] pca953x 2-0020: using no AI
[ 0.989028] omap_i2c 2010000.i2c: bus 2 rev0.12 at 400 kHz
So I2C instance is probing well.
You need to copy your custom dtb to root/boot/dtb/ti/
Then the U-boot will pick your new dtb from the above location.
- Keerthy