Part Number: SK-AM62A-LP
Tool/software:
Hello Expert,
we are using processor-sdk 10.00.1 and we have enabled ddr ecc in u-boot from the ti software-dl.ti.com/.../UG-DDRSS.html .after that we try to boot the board it was showing below error.I am providing boot log for the reference.
[ 0.000000] Call trace: [ 0.000000] create_kpti_ng_temp_pgd+0x134/0x6b0 [ 0.000000] map_kernel_segment+0xa0/0x108 [ 0.000000] paging_init+0x110/0x708 [ 0.000000] setup_arch+0x200/0x5b8 [ 0.000000] start_kernel+0x74/0x688 [ 0.000000] __primary_switched+0xbc/0xd0 [ 0.000000] Code: d1000661 eb02003f 9a9a3273 aa130000 (f9400297) [ 0.000000] ---[ end trace 0000000000000000 ]--- [ 0.000000] Kernel panic - not syncing: Attempted to kill the idle task! [ 0.000000] ---[ end Kernel panic - not syncing: Attempted to kill the idle task! ]---
Thank you,
Raj.