Hi, all
I download the source code and build the kernel and filesys for Android on Panda board.
http://www.linaro.org/downloads/
http://www.linaro.org/linaro-blog/2011/09/15/building-a-linaro-android-build-from-source/
But when boot up the board, and set the static internal ip address, I found I can't ping the board from my Linux server. But if I ping the Linux server from the baord first, it's OK. So I think this might because the board doesn't broadcast its information to the outside world when using static ip address, but when using dhcp, as it has to connection to the dhcp server to get an IP address, its status is updated in the internal network. Is there any way to confront this problem. Kind of emergency for this issue.
Thanks a lot
Touse