This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: How to use GStreamer with vx_image data

Part Number: TDA4VM


Tool/software:

Hello!

I have custom board. I do not have the screen. I have imx390 camera that is managed by RTOS on R5F core. To test my setup I use vx_app_single_camera demo. I know that it works because I captured the image, but I would like to stream the video using GStreamer. I know that TI provides gst_wrapper, but I do not know how to use it with vx_image. Is there any example application that use vx_image data as a parameter for gst_wrapper?

  • Hi Lukasz,

    Can you provide your hardware and software platform?

  • Hi Lukasz,

    I have imx390 camera that is managed by RTOS on R5F core.
    but I would like to stream the video using GStreamer.

    On TI S/W platforms, it is typically either RTOS (single-cam app) or edgeai (gstreamer), but not both.
    With edgeai, sensor driver in at the LInux side.

    I have custom board. I do not have the screen.

    Copying my friend for her comments.

  • You know, my camera is managed by RTOS, but using single cam demo, the pointer to the image is available from A72 core. so my understanding is that, I can use somehow this available data to send them by gstreamer. for now I think I could create new node, and reuse the function - after some modifications - that writes YUV420 image into file.

    vx_int32 write_output_image_fp(FILE * fp, vx_image out_image)
    {
        vx_uint32 width, height;
        vx_df_image df;
        vx_imagepatch_addressing_t image_addr;
        vx_rectangle_t rect;
        vx_map_id map_id1, map_id2;
        void *data_ptr1, *data_ptr2;
        vx_uint32 num_bytes_per_4pixels;
        vx_uint32 num_luma_bytes_written_to_file=0;
        vx_uint32 num_chroma_bytes_written_to_file=0;
        vx_uint32 num_bytes_written_to_file=0;
        vx_uint32 imgaddr_width, imgaddr_height, imgaddr_stride;
        int i;
    
        vxQueryImage(out_image, VX_IMAGE_WIDTH, &width, sizeof(vx_uint32));
        vxQueryImage(out_image, VX_IMAGE_HEIGHT, &height, sizeof(vx_uint32));
        vxQueryImage(out_image, VX_IMAGE_FORMAT, &df, sizeof(vx_df_image));
    
    
        if(VX_DF_IMAGE_NV12 == df)
        {
            num_bytes_per_4pixels = 4;
        }
        else if(TIVX_DF_IMAGE_NV12_P12 == df)
        {
            num_bytes_per_4pixels = 6;
        }
        else
        {
            num_bytes_per_4pixels = 8;
        }
    
        rect.start_x = 0;
        rect.start_y = 0;
        rect.end_x = width;
        rect.end_y = height;
    
        vxMapImagePatch(out_image,
            &rect,
            0,
            &map_id1,
            &image_addr,
            &data_ptr1,
            VX_WRITE_ONLY,
            VX_MEMORY_TYPE_HOST,
            VX_NOGAP_X
            );
    
        if(!data_ptr1)
        {
            printf("data_ptr1 is NULL \n");
            return -1;
        }
    
        imgaddr_width  = image_addr.dim_x;
        imgaddr_height = image_addr.dim_y;
        imgaddr_stride = image_addr.stride_y;
        printf("imgaddr_width = %d \n", imgaddr_width);
        printf("imgaddr_height = %d \n", imgaddr_height);
        printf("imgaddr_stride = %d \n", imgaddr_stride);
        printf("width = %d \n", width);
        printf("height = %d \n", height);
    
        num_luma_bytes_written_to_file = 0;
    
        for(i=0;i<height;i++)
        {
            num_luma_bytes_written_to_file  += fwrite(data_ptr1, 1, width*num_bytes_per_4pixels/4, fp);
            data_ptr1 += imgaddr_stride;
        }
        vxUnmapImagePatch(out_image, map_id1);
    
        fflush(fp);
    
    
        if(VX_DF_IMAGE_NV12 == df || TIVX_DF_IMAGE_NV12_P12 == df)
        {
            vxMapImagePatch(out_image,
                &rect,
                1,
                &map_id2,
                &image_addr,
                &data_ptr2,
                VX_WRITE_ONLY,
                VX_MEMORY_TYPE_HOST,
                VX_NOGAP_X
                );
    
            if(!data_ptr2)
            {
                printf("data_ptr2 is NULL \n");
                return -1;
            }
    
            imgaddr_width  = image_addr.dim_x;
            imgaddr_height = image_addr.dim_y;
            imgaddr_stride = image_addr.stride_y;
    
            num_chroma_bytes_written_to_file = 0;
            for(i=0;i<imgaddr_height/2;i++)
            {
                num_chroma_bytes_written_to_file  += fwrite(data_ptr2, 1, imgaddr_width*num_bytes_per_4pixels/4, fp);
                data_ptr2 += imgaddr_stride;
            }
    
            fflush(fp);
    
            vxUnmapImagePatch(out_image, map_id2);
        }
    
        num_bytes_written_to_file = num_luma_bytes_written_to_file + num_chroma_bytes_written_to_file;
        printf("Written %d bytes \n", num_bytes_written_to_file);
    
        return num_bytes_written_to_file;
    }

    I think next I could use this buffer as an input for  appGstSrcInit / appCodecSrcInit function.

  • Lukasz,

    You know, my camera is managed by RTOS, but using single cam demo, the pointer to the image is available from A72 core. so my understanding is that, I can use somehow this available data to send them by gstreamer.

    I don't think TI SDK has that implemented/tested.
    There could be quite some S/W changes required at gstreamer module/plugin level, but I am not familiar with those S/W details.

    Copying my friends and for their comments.