This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM625SIP: AM625 PWM Support

Part Number: AM625SIP

Tool/software:

Hi TI Experts,

Based on our use case, I need to control 12 individual LEDs using the AM62x SOC.

Referring to the AM62x datasheet, I see that EPWM0, EPWM1, and EPWM2 can each function as dual-channel PWM outputs, and ECAP0, ECAP1, and ECAP2 can each be configured as single-channel PWM outputs. This configuration provides a total of 9 PWM outputs.

I'd like to inquire is it's possible to configure other EPHRPWM signal pins, such as the EPWM SOC, trip zone input pins, and syncio pins, as single-channel PWM outputs as well.

Please clarify.

Thanks & Regards 

Kaliga Devi S