This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

J722SXH01EVM: [J722S][EVM] how to set boot mode to eMMC ?

Part Number: J722SXH01EVM

Tool/software:

Hi TI,

[J722S][EVM] how to set boot mode to eMMC ?

software-dl.ti.com/.../J722S_EVM_Hardware_Setup.html
Switch settings
Bootmodes are selected using the SW3 and SW4 switches on the EVM. Most common boot method is to use SD card.
Following are the switch settings to set the boot mode to SD for the EVM.
SW3[1:8] = 1100 0010 SW4[1:8] = 0100 0000

>> this is SD card boot,  I tested this, evm can boot into linux success+.

Thanks
Jiahao