Other Parts Discussed in Thread: DA8XX
Tool/software:
SDK_VER : 10_00_00
I tried use uboot-flash-writer to burn the AM62A7 chip based on the linked doc, but it threw an error.Here's the log
3.1.1.2. USB Device Firmware Upgrade (DFU) — Processor SDK AM62Ax Documentation
U-Boot SPL 2024.04-dirty (May 16 2025 - 09:51:01 +0800) SYSFW ABI: 4.0 (firmware rev 0x000a '10.0.8--v10.00.08 (Fiery Fox)') SPL initial stack usage: 13568 bytes SPL: failed to boot from all boot devices ### ERROR ### Please RESET the board ###
The uboot configs/am62ax_evm_a53_defconfig is as follow
CONFIG_ARM=y CONFIG_ARCH_K3=y CONFIG_SYS_MALLOC_F_LEN=0x8000 CONFIG_SPL_GPIO=y CONFIG_SPL_LIBCOMMON_SUPPORT=y CONFIG_SPL_LIBGENERIC_SUPPORT=y CONFIG_NR_DRAM_BANKS=2 CONFIG_SOC_K3_AM62A7=y CONFIG_TARGET_AM62A7_A53_EVM=y CONFIG_HAS_CUSTOM_SYS_INIT_SP_ADDR=y CONFIG_CUSTOM_SYS_INIT_SP_ADDR=0x80480000 CONFIG_DM_GPIO=y CONFIG_ENV_SIZE=0x40000 CONFIG_SPL_DM_SPI=y CONFIG_DEFAULT_DEVICE_TREE="k3-am62a7-sk" CONFIG_SPL_TEXT_BASE=0x80080000 CONFIG_OF_LIBFDT_OVERLAY=y CONFIG_SF_DEFAULT_SPEED=25000000 CONFIG_DM_RESET=y CONFIG_SPL_MMC=y CONFIG_SPL_SERIAL=y CONFIG_SPL_STACK_R_ADDR=0x82000000 CONFIG_SPL_FS_FAT=y CONFIG_SPL_LIBDISK_SUPPORT=y CONFIG_SPL_SPI=y # CONFIG_SYS_MALLOC_CLEAR_ON_INIT is not set CONFIG_SPL_LOAD_FIT=y CONFIG_SPL_LOAD_FIT_ADDRESS=0x81000000 CONFIG_BOOTSTD_FULL=y CONFIG_BOARD_LATE_INIT=y CONFIG_SPL_MAX_SIZE=0x58000 CONFIG_SPL_PAD_TO=0x0 CONFIG_SPL_HAS_BSS_LINKER_SECTION=y CONFIG_SPL_BSS_START_ADDR=0x80a00000 CONFIG_SPL_BSS_MAX_SIZE=0x80000 CONFIG_SPL_SYS_MALLOC_SIMPLE=y CONFIG_SPL_STACK_R=y CONFIG_SYS_MMCSD_RAW_MODE_U_BOOT_USE_SECTOR=y CONFIG_SYS_MMCSD_RAW_MODE_U_BOOT_SECTOR=0x1400 CONFIG_SPL_ENV_SUPPORT=y CONFIG_SPL_FS_LOAD_PAYLOAD_NAME="u-boot.img" CONFIG_SPL_I2C=y CONFIG_SPL_DM_MAILBOX=y CONFIG_SPL_MTD=y CONFIG_SPL_MTD_LOAD=y CONFIG_SYS_MTD_U_BOOT_OFFS=0x280000 CONFIG_CMD_NFS=y CONFIG_SPL_NAND_SPI_SUPPORT=y CONFIG_SPL_DM_SPI_FLASH=y CONFIG_SPL_POWER_DOMAIN=y CONFIG_SPL_YMODEM_SUPPORT=y CONFIG_CMD_MMC=y CONFIG_CMD_USB_MASS_STORAGE=y CONFIG_CMD_DDRSS=y CONFIG_CMD_MTD=y CONFIG_CMD_MTDPARTS=y CONFIG_CMD_UBI=y CONFIG_OF_CONTROL=y CONFIG_SPL_OF_CONTROL=y CONFIG_MULTI_DTB_FIT=y CONFIG_SPL_MULTI_DTB_FIT=y CONFIG_SPL_MULTI_DTB_FIT_NO_COMPRESSION=y CONFIG_SPL_DM=y CONFIG_SPL_DM_DEVICE_REMOVE=y CONFIG_SPL_DM_SEQ_ALIAS=y CONFIG_REGMAP=y CONFIG_SPL_REGMAP=y CONFIG_SPL_SYSCON=y CONFIG_SYSCON=y CONFIG_SPL_OF_TRANSLATE=y CONFIG_CLK=y CONFIG_SPL_CLK=y CONFIG_CLK_TI_SCI=y CONFIG_DFU_SF=y CONFIG_DFU_MTD=y CONFIG_DMA_CHANNELS=y CONFIG_TI_K3_NAVSS_UDMA=y CONFIG_TI_SCI_PROTOCOL=y CONFIG_SPL_DM_GPIO_LOOKUP_LABEL=y CONFIG_DA8XX_GPIO=y CONFIG_DM_PCA953X=y CONFIG_SPL_DM_PCA953X=y CONFIG_DM_I2C=y CONFIG_SYS_I2C_OMAP24XX=y CONFIG_DM_MAILBOX=y CONFIG_K3_SEC_PROXY=y CONFIG_SUPPORT_EMMC_BOOT=y #CONFIG_MMC_IO_VOLTAGE=y #CONFIG_SPL_MMC_IO_VOLTAGE=y #CONFIG_MMC_UHS_SUPPORT=y #CONFIG_SPL_MMC_UHS_SUPPORT=y CONFIG_MMC_HS200_SUPPORT=y CONFIG_SPL_MMC_HS200_SUPPORT=y CONFIG_MMC_SDHCI=y CONFIG_MMC_SDHCI_ADMA=y CONFIG_SPL_MMC_SDHCI_ADMA=y CONFIG_MMC_SDHCI_AM654=y CONFIG_MTD=y CONFIG_DM_MTD=y CONFIG_MTD_SPI_NAND=y CONFIG_PHY_TI_DP83867=y CONFIG_PHY_FIXED=y CONFIG_TI_AM65_CPSW_NUSS=y CONFIG_PHY=y CONFIG_PINCTRL=y CONFIG_SPL_PINCTRL=y CONFIG_PINCTRL_SINGLE=y CONFIG_POWER_DOMAIN=y CONFIG_TI_SCI_POWER_DOMAIN=y #CONFIG_DM_REGULATOR=y #CONFIG_SPL_DM_REGULATOR=y #CONFIG_DM_REGULATOR_FIXED=y #CONFIG_SPL_DM_REGULATOR_FIXED=y #CONFIG_DM_REGULATOR_GPIO=y #CONFIG_SPL_DM_REGULATOR_GPIO=y CONFIG_K3_SYSTEM_CONTROLLER=y CONFIG_REMOTEPROC_TI_K3_ARM64=y CONFIG_REMOTEPROC_TI_K3_R5F=y CONFIG_REMOTEPROC_TI_K3_DSP=y CONFIG_RESET_TI_SCI=y CONFIG_DM_SERIAL=y CONFIG_SOC_DEVICE=y CONFIG_SOC_DEVICE_TI_K3=y CONFIG_SOC_TI=y CONFIG_SPI=y CONFIG_DM_SPI=y CONFIG_CADENCE_QSPI=y CONFIG_SYSRESET=y CONFIG_SPL_SYSRESET=y CONFIG_SYSRESET_TI_SCI=y CONFIG_DM_THERMAL=y CONFIG_FS_FAT_MAX_CLUSTSIZE=16384 CONFIG_DM_SPI_FLASH=y CONFIG_CMD_REMOTEPROC=y CONFIG_SYS_MALLOC_LEN=0x2000000 CONFIG_SPL_BOARD_INIT=y #CONFIG_MMC_TRACE=y #include <configs/am62x_a53_usbdfu.config> #include <configs/am62x_a53_usbmsc.config> CONFIG_ENV_IS_NOWHERE=y CONFIG_BOOTDELAY=0 CONFIG_BOOTCOMMAND="setenv dfu_alt_info_flashenv uEnv.txt ram 0x82000000 0x10000000; setenv dfu_alt_info ${dfu_alt_info_flashenv}; dfu 0 ram 0; env import -t ${loadaddr} $filesize; run user_commands;"
The tools/DFU_flash/bin/am62axx-evm/hsfs/flash-files.cfg is as follow
# R5F SPL @Raw flash to Boot0 hardware partition --file=/home/flork/sdk/ti-processor-sdk-linux-edgeai-am62a-evm-10_00_00_08/board-support/ti-u-boot-2024.04+git/build/r5/tiboot3-am62ax-hs-fs-evm.bin --operation=flash-emmc --flash-offset=0x0 --attributes="raw,1,-" # A53 SPL @Raw flash to Boot0 hardware partition --file=/home/flork/sdk/ti-processor-sdk-linux-edgeai-am62a-evm-10_00_00_08/board-support/ti-u-boot-2024.04+git/build/a53/tispl.bin --operation=flash-emmc --flash-offset=0x80000 --attributes="raw,1,-" # A53 U-Boot @Raw flash to Boot0 hardware partition --file=/home/flork/sdk/ti-processor-sdk-linux-edgeai-am62a-evm-10_00_00_08/board-support/ti-u-boot-2024.04+git/build/a53/u-boot.img --operation=flash-emmc --flash-offset=0x280000 --attributes="raw,1,-" # # Rootfs @Raw flash to GPT or DOS partition 1 in UDA hardware partition --file=/home/flork/sdk/ti-processor-sdk-linux-edgeai-am62a-evm-10_00_00_08/filesystem/tisdk-tiny-image.img --operation=flash-emmc --flash-offset=0x0 --attributes="part,0,2"
The filesystem was created by dd if=/dev/null of=tisdk-tiny-image.img bs=1M seek=250