Other Parts Discussed in Thread: TPS65910, TPS65910A, TPS51200, TPS51206, AM3359
I'd like to use the TPS65910B to power the AM335x on a project. Can the TPS65910B's VRTC output be used to power the AM335X's VRTC? In the AM335x reference designs, an additional regulator is always added to power the RTC instead of using the VRTC from the TPS65910. I'd rather not have to add an additional regulator if the one already in the PMIC will work.
Also, is there a reference design for the AM335x with the TPS65910B and DDR3? Or are there any AM335x/DDR3 routing rules?
thanks