This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C64+ JPEG decoder error

HI

One of our customers is using JPEG_PS_Decoder_C64XPLUS ver 02_00_02 (obtained from http://software-dl.ti.com/dsps/dsps_public_sw/codecs/C64XPlus_Video/index_FDS.html)  on a custom DM6443-based board. They are getting an error, the transcript of which is given below. The working environment is gstreamer + DVSDK 2.0 + Linux. Please provide any pointers on what the issue could be.

regards

Abhilash

#gst-launch filesrc location=baby-krish-640x480.jpg ! TIImgdec1 resolution=640x480 ! filesink location=/tmp/jpeg.uyvy

@0x0004f5d9:[T:0x40048000] ti.sdo.dmai - [Dmai] Dmai log level set to '2'. Note that calling CERuntime_init after this point may cause unexpected change to DMAI tracin.
Setting pipeline to PAUSED ...
Pipeline is PREROLLING ...
@0x00107a6e:[T:0x41eed490] ti.sdo.dmai - [Idec1] Image decoder instance created
@0x00107f1c:[T:0x41eed490] ti.sdo.dmai - [Idec1] Buffer size 307200 obtained from XDM_GETBUFINFO control call
@0x001085db:[T:0x41eed490] ti.sdo.dmai - [Buffer] Alloc Buffer of size 1075200 at 0x42857000 (0x8d4fe000 phys)
@0x001088e4:[T:0x41eed490] ti.sdo.dmai - [BufTab] Allocating BufTab for 1 buffers
@0x001089e7:[T:0x41eed490] OM - Memory_contigAlloc> Warning: non-default alignment not supported for pool-based allocations, using default 0xffffffff.
@0x00108bd7:[T:0x41eed490] ti.sdo.dmai - [Buffer] Alloc Buffer of size 614400 at 0x42d62000 (0x8d368000 phys)
@0x0010b533:[T:0x41eed490] ti.sdo.dmai - [Buffer] Set user pointer 0x42857000 (physical 0x8d4fe000)
@0x0010b79e:[T:0x41eed490] ti.sdo.dmai - [Buffer] Set user pointer 0x42857000 (physical 0x8d4fe000)
@0x0010b93e:[T:0x41eed490] ti.sdo.dmai - [ColorSpace] Unknown color space format (-1)
Pipeline is PREROLLED ...
Setting pipeline to PLAYING ...
@0x00119431:[T:0x41eed490] ti.sdo.dmai - [Buffer] Set user pointer 0x4286e3a7 (physical 0x8d5153a7)
@0x001196df:[T:0x41eed490] ti.sdo.dmai - [Buffer] Free Buffer of size 1075200 at 0x42857000 (0x8d4fe000 phys)
@0x0011acae:[T:0x41eed490] ti.sdo.dmai - [Buffer] Free Buffer of size 614400 at 0x42d62000 (0x8d368000 phys)
New clock: GstSystemClock
Got EOS from element "pipeline0".
Execution ended after 2685407 ns.
Setting pipeline to PAUSED ...
Setting pipeline to READY ...
Setting pipeline to NULL ...
Freeing pipeline ...