This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VEN-Q1: Regarding the necessity of the VPP power supply

Part Number: TDA4VEN-Q1


Tool/software:

Hi, TI.

If only software writing using a debugger is assumed, is the VPP power supply necessary?

If not needed, I plan not to implement the VPP power supply line on the board.

#I expected to be necessary when used for OTA (Over-The-Air) update

  • VPP is only necessary when programming security keys in the device.  It It is not needed for booting or during normal execution.  It is not needed normally when doing software update (OTA) either.  It is also not needed if not using the security features of the device.